STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

F2/F4 I2S Ext.Clock

Posted on April 03, 2013 at 14:19Hi friends, It is written at ref/man for F2 and F4:Bit 7:0 I2SDIV: I2S Linear prescaler I2SDIV [7:0] = 0 or I2SDIV [7:0] = 1 are forbidden values. Why ''0'' is forbidden is clear, but why ''1'' ?! I make some intensi...

Using RTC to show time on LCD

Posted on April 04, 2013 at 11:52Hello,I'm new to embedded programming and having a hard time getting into using the STM32L-Discovery. I'm trying to use the RTC to display time on the LCD on the board, I've been reading the documentation but haven't...

Best TCP/IP Stack for STM32F2

Posted on April 03, 2013 at 21:46HI, I'm going to extend my project with TCP/IP stack. What do you think is a best choice for TCP/IP stack. Currently I'm hesitating between lwIP and uIP.  I'm developing under yagarto. Currently my code runs FreeRTO...

dimax by Senior
  • 2105 Views
  • 4 replies
  • 0 kudos

Timer problem

Posted on April 05, 2013 at 03:40Hi guysI want to do an experience with stm32f4.I want to simulate AM(amplitude modulation).I want to use 168 MHz as a carrier and generate the data in 100 khz. and modulate this 2 waves together.this action like i pu...

imanpakii by Associate III
  • 1036 Views
  • 1 replies
  • 0 kudos

JTAG Boundary Scan with ScanExpress

Posted on April 04, 2013 at 22:17My company uses a nifty tool called ScanExpress that takes your netlist, parts list, and BSDL files for the JTAG chain and creates an automated test using the Boundary scan to see if all the connections are correct. ...

wmoyne by Associate II
  • 940 Views
  • 0 replies
  • 0 kudos

Missing ADC Codes on STM32F1 / ADC3

Posted on April 04, 2013 at 17:37Hi all,      When I supply 2 of my ADC inputs with 3V ramp/triangle/sine waves, it seems that values from 1024 - 1048 are reporting as 1023.  There is another smaller ''dead band'' from 1087 up to 1092.  Everything e...

diydsp by Associate
  • 1287 Views
  • 1 replies
  • 0 kudos

Fast floating point math

Posted on April 03, 2013 at 11:27Hello, i run in to a problem, where i need to do math with single precision floating point. it looks like if(...) condition, and printing floating point to uint16_t is very slow. so i have two questions: first, what ...

linas2 by Associate II
  • 11978 Views
  • 25 replies
  • 0 kudos

RAM duration : erased at reset ?

Posted on April 04, 2013 at 15:51Hello ST lovers,I have a very simple yet critical to my project question : is the RAM in the STM32F405 erased upon reset ? If yes, then is there any EEPROM I can use to store 32 bits of data that'll survive through r...

STM32F2xx FLASH erease program

Posted on April 04, 2013 at 14:43I have problem erease the write to the FLASH . I do as follow    FLASH_Unlock();    FLASH_EraseSector(FLASH_Sector_4, VoltageRange_3); Prair to that I check that all  section are unlock nWRP= 0xFFF. I use HSE and I ...

Barbie by Associate II
  • 1251 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.