2013-05-11 1:43 AM
hello my sth32f4 discovery is mcu is running hot and u1 is hot also what is going on??
2013-05-11 5:42 AM
How hot would that be? In units of C or F, or how long your figure can dwell without burning/pain?
What was happening prior to this condition being observed? High voltages, exceeding operating frequency, high load, shorts? Does it persist if you reset with BOOT[0] High?2013-05-12 4:12 AM
i was using the adc and i think i shorted 12v to the adc there is a lot of noise on the adc now .
boot did not fix the problem and i can run the board for about 30-40 seconds before i have to remove my finger2013-05-12 1:19 PM
Does not sound good - but damage may be confined just to that single ADC pin. (we hope you limited the application of ''illegal'' excess voltage to just one pin)
We've been guilty - many others too - but in our case - no more. Our solution was to design a multi-channel, voltage-clamped, buffer/op-amp board - which is unable to output beyond 3V3 to our MCUs under test. We have voltage clamps on both every input channel and redundantly (for safety) upon every output channel. And - should our circuit detect an over-voltage condition - we immediately open a power FET which routes all voltages to our buffer/op-amp board. Not quite to ''space station'' or ''human implantation'' standards - but ''good for Gov't work - in most cases.'' Now in your case - check/double check that the 12V has been safely/properly divided down to ''MCU appropriate'' levels. Suggest that you remove all signals from that suspect pin (recipient of your over-voltage) - does the MCU still over-heat? And - ''finger method'' of heat measure may introduce ESD - along with not providing an ''overly exact/repeatable'' measurement. If you're lucky - you may be able to salvage many/most of the MCU's other pins. A good measure of the MCU's health may be its current draw - prior to and after abuse. A second M4 demo board enables such a, ''baseline'' measure...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.