STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 HS USB DMA Transfer

Posted on May 14, 2013 at 23:02Is it possible to use DMA for USB transfers? My understanding of the STM32 DMA controller is that it will transfer data from one place to another without CPU usage. If I were moving data from RAM to a DAC output, I can...

ckern by Associate II
  • 3091 Views
  • 3 replies
  • 0 kudos

STM32F4xx Bootloader and Security

Posted on June 15, 2013 at 13:18I wrote my bootloader, that load application to the flash. Now I want to set security. Is it enough to set RDP Level1 and write protection to sector0, where my bootloader is located? Or I need to set RDP to Level2? Th...

alexandr by Associate II
  • 1287 Views
  • 2 replies
  • 0 kudos

How to define the GPIO mode ?

Posted on August 13, 2012 at 09:20typedef enum { GPIO_Mode_AIN = 0x0,   GPIO_Mode_IN_FLOATING = 0x04,   GPIO_Mode_IPD = 0x28,   GPIO_Mode_IPU = 0x48,   GPIO_Mode_Out_OD = 0x14,   GPIO_Mode_Out_PP = 0x10,   GPIO_Mode_AF_OD = 0x1C,   GPIO_Mode_AF_PP =...

614678489 by Associate II
  • 9784 Views
  • 10 replies
  • 0 kudos

WiFi query

Posted on March 12, 2013 at 06:40Hi, Anyone of you have worked on WIFI? I need a small help related to that. I am using Hi-Link WIFI module named HLK M03 WIFI module with STM32 controller. I am able to configure my WIFI module properly i.e. initiali...

manoj23 by Associate II
  • 3633 Views
  • 10 replies
  • 0 kudos

Problem with erasing and overwriting FLASH data

Posted on June 15, 2013 at 12:58Hi,After writing in FLASH using FLASH_ProgramWord(uint32_t Address,Data). I can't overwrite that address data completely using FLASH_ProgramWord(Address,0xFFFFFFFF) or FLASH_ProgramWord(Address,Newdata);.In case of er...

Using ST FSMC_SRAM_DataMemory example on keil

Posted on June 14, 2013 at 12:41I cannot find the startup file and scatter file for Keil for FSMC_SRAM_DataMemory example in STM32F4xx_DSP_StdPeriph_Lib_V1.1.0.Basically i want to use external memory on STM3240G eval  board as my stack and heap spac...

rishi2 by Associate III
  • 2380 Views
  • 4 replies
  • 0 kudos

ADC GPIO pin pairing for STM32F407

Posted on June 14, 2013 at 23:22Can someone tell me the paring for all ADC channels and GPIO ports for the STM32F407? I've seen some of the pairings in posts here (such as PA0 for channel 0, CA2 for channel 12), but I need a complete list. I'm sorry...

cwparker by Associate II
  • 1349 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.