2013-07-01 9:08 PM
i have a problem with recieve data to stm32. send data to UART works fine in hyperterminal on windows i see all wordl who send stm32.
But we need
to
STM32
could
also
receive data
from the computer.
I need
to
able to
recognize the signs
+, -
, Enter,delete
and
after the adoption
of the character
performed
the function.
Defining
UART
ok
I
do not know how
to make a program
to receive the data
.
Thank you all
for your advice
#recieve-uart2013-07-01 9:31 PM
Well you could receive the data into a line buffer, and then parse it, or perhaps use a state machine if you want to deal with it a character at a time.
The data presumably will be sent as 8-bit bytes, you can load them into a char, or an array of chars. The DR is 16-bit to permit the reception of 9-bit data in such modes that permit that, those can be safely ignored for HyperTerminal, or other better terminal apps. Perhaps a review of sscanf(), strstr(), strtok() might be in order?2013-07-02 4:02 AM
I thought
that would be the
: xxx=
Received
(
Usart1)..
but do not know
how
to
write
.I've already
tried with
many options.
And the back
does not work
.Help me please
.sending
data
works for me
.Way back
no
Thanks
i
work in
stm32f3
discovery
kit
Sorry for
my English
..
I am
from the Czech Republic
2013-07-02 4:52 AM
while(USART_GetFlagStatus(USARTx, USART_FLAG_RXNE) == RESET);
RxBuffer[RxIndex++] = USART_ReceiveData(USARTx);2013-07-03 9:26 PM
Hi,
Thanks for the advice
.it works.
Now we can
tell
when you come
STM32
any
character
.RxIndex
can compute
and send
back to the PC
how many characters
came
.but
still
I can not
convert
RxBuffer
the word that
I
sent
back
to the PC.
or
able to
recognize
what kind of
character.
Thank you
for your advice
.
2013-07-12 2:17 AM
Hi please help me. How do I
detect incoming
character from
pc
and the next
step
to do
that
then
do
some
processing
cycle
according to
the
character.
For example,
if (
receivechar
==
+)
{
pk1
+ +
;}
if (
receivechar== -
) {
=
pok
pok
-
PK1;}
2013-07-12 4:52 AM
If
compilers encoding (file's encoding) and character encoding from PC is same, then your example if statements should work. However... I would rather send certain binary data...2013-07-12 10:59 AM
This all sounds like high school level C programming issues, it's probably a generational thing, I didn't grow up with windows and dialogs.
Here's how I might create a simple calculator app on the F4, as I don't have a USART hung off my F3 board. The concepts should be pretty portable.// STM32 Simple Calculator USART2 (Tx PA.2, Rx PA.3) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); // USART2_TX
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2); // USART2_RX
}
/**************************************************************************************/
void USART2_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_Cmd(USART2, ENABLE);
}
/**************************************************************************************/
char USART_GetChar(void)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); // Wait for Full
return((char)USART_ReceiveData(USART2));
}
/**************************************************************************************/
void USART_PutChar(char i)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, i);
}
/**************************************************************************************/
void USART_PutString(char *s)
{
while(*s)
USART_PutChar(*s++);
}
/**************************************************************************************/
void USART_PutDecimal(int i)
{
char str[16], *s;
int n;
s = str + sizeof(str); // Point to tail
*--s = 0; // NUL
if (i <
0
) // Negative
{
n
=
1
;
i = -i; // Negate
}
else
n
=
0
;
do
{
*
--s
=
'0'
+ (char)(i % 10);
i
= i / 10;
}
while(i);
if (n) // Add sign if negated
*
--s
=
'-'
;
USART_PutString(s);
}
/**************************************************************************************/
void USART_Calc(void) // Simple Calculator from keystrokes
{
int accum, num;
char i;
accum
=
0
;
num
=
0
;
while(1)
{
i
=
USART_GetChar
();
if ((i >= '0') && (i <= '9')) // Decimal?
{
num = (num * 10) + (int)(i - '0'); // Load the number
}
else if (i == '+')
{
accum += num; // add
num = 0; // clear
USART_PutDecimal(accum);
USART_PutString(''
'');
}
else if (i == '-')
{
accum -= num; // subtract
num = 0; // clear
USART_PutDecimal(accum);
USART_PutString(''
'');
}
else if (i == '.') // Print current accumulator and number
{
USART_PutString(''accum:'');
USART_PutDecimal(accum);
USART_PutString('', num:'');
USART_PutDecimal(num);
USART_PutString(''
'');
}
}
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART2_Configuration();
USART_Calc();
while(1); // Don't want to exit
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.