2013-07-17 7:17 PM
Hi,everyone
I have a question about SDADC and DMA.when Ienable
the DMA with'' DMA_Cmd(DMA2_Channel3, ENABLE)'' in program and the SDADC1 stop convert immediately. here is my code:void SDADC1_Config()
{ SDADC_InitTypeDef SDADC_InitStructure; SDADC_AINStructTypeDef SDADC_AINStructure; GPIO_InitTypeDef GPIO_InitStructure; uint32_t SDADCTimeout = 0; RCC_APB2PeriphClockCmd(RCC_APB2Periph_SDADC1, ENABLE); SDADC_DeInit(SDADC1); /* PWR APB1 interface clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); /* Enable SDADC analog interface */ PWR_SDADCAnalogCmd(PWR_SDADCAnalog_1, ENABLE); /* Set the SDADC divider: The SDADC should run @6MHz */ /* If Sysclk is 72MHz, SDADC divider should be 12 */ RCC_SDADCCLKConfig(RCC_SDADCCLK_SYSCLK_Div12); /* GPIO Peripheral clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE); /* SDADC channel 3P pin configuration: PE7 */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOE, &GPIO_InitStructure); /* Select External reference: The reference voltage selection is available only in SDADC1 and therefore to select the VREF for SDADC2/SDADC3, SDADC1 clock must be already enabled */ SDADC_VREFSelect(SDADC_VREF_Ext); /* Insert delay equal to ~5 ms */ // Delay(2); SDADC_Cmd(SDADC1, ENABLE); SDADC_InitModeCmd(SDADC1, ENABLE); SDADCTimeout = 30; /* wait for INITRDY flag to be set */ while((SDADC_GetFlagStatus(SDADC1, SDADC_FLAG_INITRDY) == RESET) && (--SDADCTimeout != 0)); // if(SDADCTimeout == 0) // { // /* INITRDY flag can not set */ // return 1; // } SDADC_AINStructure.SDADC_InputMode =SDADC_InputMode_SEOffset; //SDADC_InputMode_SEZeroReference; SDADC_AINStructure.SDADC_Gain = SDADC_Gain_1_2;//GAIN is 0.5 SDADC_AINStructure.SDADC_CommonMode = SDADC_CommonMode_VSSA; SDADC_AINStructure.SDADC_Offset = 0; SDADC_AINInit(SDADC1, SDADC_Conf_0, &SDADC_AINStructure); /* Channel3 configuration */ SDADC_InitStructure.SDADC_Channel = SDADC_Channel_3; SDADC_InitStructure.SDADC_ContinuousConvMode = ENABLE; SDADC_InitStructure.SDADC_FastConversionMode = DISABLE; SDADC_Init(SDADC1, &SDADC_InitStructure); SDADC_DMAConfig(SDADC1,SDADC_DMATransfer_Regular, ENABLE); SDADC_ChannelConfig(SDADC1, SDADC_Channel_3, SDADC_Conf_0); SDADC_InitModeCmd(SDADC1, DISABLE); /* configure calibration to be performed on conf0 */ SDADC_CalibrationSequenceConfig(SDADC1, SDADC_CalibrationSequence_1); /* start PT100_SDADC Calibration */ SDADC_StartCalibration(SDADC1); /* Set calibration timeout: 5.12 ms at 6 MHz in a single calibration sequence */ SDADCTimeout = 4*30720 ; /* wait for PT100_SDADC Calibration process to end */ while((SDADC_GetFlagStatus(SDADC1, SDADC_FLAG_EOCAL) == RESET) && (--SDADCTimeout != 0)); // if(SDADCTimeout == 0) // { // /* EOCAL flag can not set */ // return 2; // } // /* SDADC successfully configured */ // return 0; SDADC_SoftwareStartConv(SDADC1); } void DMA2_Configuration(void) { DMA_InitTypeDef DMA_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable DMA2 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2, ENABLE); /* Config the DMA2 channel 3 */ DMA_DeInit(DMA2_Channel3); DMA_InitStructure.DMA_PeripheralBaseAddr = ((uint32_t)&SDADC1->RDATAR); DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&Volt_Buffer; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC; DMA_InitStructure.DMA_BufferSize = N; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_Low; DMA_InitStructure.DMA_M2M = DMA_M2M_Disable; DMA_Init(DMA2_Channel3, &DMA_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = DMA2_Channel3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 3; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Enable DMA2 Channel3 Transfer half and Complete interrupt */ DMA_ITConfig(DMA2_Channel3, DMA_IT_TC , ENABLE); /* Enable DMA2 Channel3 */ DMA_Cmd(DMA2_Channel3, ENABLE); } Who can tell me,how to use 16bit SDADC with DMA??2013-07-17 7:58 PM
Unfortunately the code is insufficiently complete to really evaluate.
One line does trouble me, and suspect it causes the DMA to fault. DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&Volt_Buffer; I don't see a definition for the buffer but assume it's uint16_t Volt_Buffer[N]; The correct code would be DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&Volt_Buffer[0]; or DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)Volt_Buffer;2013-07-17 8:22 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.