STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART and Hyperterminal

Posted on July 31, 2013 at 11:55 Hi, I create on my stm3220G evaluation board an example with USART. The code: #include < stm32f2xx.h > #include < misc.h > // I recommend you have a look at these in the ST firmware folder #include < st...

mosine by Associate II
  • 1298 Views
  • 6 replies
  • 0 kudos

Timer related general questions

Posted on July 31, 2013 at 12:331. What is total delay produced by timer in STM32f205:delay =  (   (ARR+1) * (PSC+1) )  / Timer_freq               or delay =  (   (ARR) * (PSC+1) )  / Timer_freq                   ordelay =  (   (ARR) * (PSC) )  / Ti...

Drive low TIM output in not active state

Posted on July 16, 2013 at 14:24I have STM32F4-discovery board. And I use code from example to configure PWM output. Chapter 14.4.9 TIMx capture/compare enable register (TIMx_CCER) of RM0090:   Bit 0 CC1E: Capture/Compare 1 output enable.     CC1 ch...

glory_man by Associate II
  • 1285 Views
  • 1 replies
  • 0 kudos

USB Audio Asynchronous Source endpoint won't sync...

Posted on July 25, 2013 at 19:22Hello everyone, I'm currently working on a USB application on a STM32F103, using the Audio Class, and after some work and extensive reading (USB specification and Audio Class specification of course, + several example...

Can usart break? stm32f0Discovery

Posted on July 30, 2013 at 10:23I connect USART1 or 2 via adapter Usb2Com but the terminal displays strange symbols....&sharpinclude ''stm32f0xx.h''&sharpinclude ''stm32f0xx_rcc.h''&sharpinclude ''stm32f0xx_gpio.h''&sharpinclude ''stm32f0xx_usart.h'...

stivcrc by Associate
  • 2171 Views
  • 4 replies
  • 0 kudos

Core is locked up

Posted on July 29, 2013 at 07:53Hi all,I am working on STM32F407ZET6 controller. I am facing problems after downloading code into the controller, it shows some error messages. When i download my code into the controller using J-Link and when i press...

manoj23 by Associate II
  • 2628 Views
  • 4 replies
  • 0 kudos

SPI with DMA is not working on STM32f2..

Posted on July 30, 2013 at 10:16Hi all,I am having problems with configuring DMA for SPI ( SPI is working without DMA).Did anyone use  DMA with SPI3 on SMT32F2 ? Pls help me figuring out the issue...here is my DMA code:Problem:It is looping @ while ...

STM32F100RB - TIM15IRQ problem

Posted on July 30, 2013 at 12:06Hello! I have problem with this line in my application with STM32F100VLDiscovery: NVIC_EnableIRQ(TIM15_IRQn); I have error - TIM15_IRQn undeclared. I did try also - NVIC_EnableIRQ(TIM15_UP_IRQn); - error again; I don'...

alprof by Associate II
  • 2801 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.