2013-07-31 2:55 AM
Hi,
I create on my stm3220G evaluation board an example with USART. The code:#include <
stm32f2xx.h
>
#include <
misc.h
> // I recommend you have a look at these in the ST firmware folder
#include <
stm32f2xx_usart.h
> // under Libraries/STM32F4xx_StdPeriph_Driver/inc and src
#include ''stm32f2xx_gpio.h''
volatile char StringLoop[] = ''The quick brown fox jumps over the lazy dog\r\n'';
//**************************************************************************************
int main(void)
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1);
/* USART1 Rx */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* USART1 Tx */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Enable USART1 IRQ */
NVIC_ClearPendingIRQ(USART1_IRQn);
NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_ITConfig(USART1, USART_IT_TXE, ENABLE);
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
USART_Cmd(USART1,ENABLE);
while(1); // Don't want to exit
}
//**************************************************************************************
void USART1_IRQHandler(void)
{
static int tx_index = 0;
static int rx_index = 0;
if (USART_GetITStatus(USART1, USART_IT_TXE) != RESET) // Transmit the string in a loop
{
USART_SendData(USART1, StringLoop[tx_index++]);
if (tx_index >= (sizeof(StringLoop) - 1))
tx_index = 0;
}
if (USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) // Received characters modify string
{
StringLoop[rx_index++] = USART_ReceiveData(USART1);
if (rx_index >= (sizeof(StringLoop) - 1))
rx_index = 0;
}
}
When I use hyperterminal, I don't see anything. why?? I set hyperterminal with the same properties of USART.
THANKS
2013-07-31 5:00 AM
I create on my stm3220G evaluation board an example with USART. When I use hyperterminal, I don't see anything. why?? I set hyperterminal with the same properties of USART.
Probably because the board uses USART3 on PC10/11?2013-07-31 5:25 AM
THANKS clive1. I changed and it works. GPIOC9 RX e GPIOC10 TX.
2013-07-31 5:34 AM
THANKS clive1. I changed and it works. GPIOC9 RX e GPIOC10 TX.
USART3_RX is PC112013-07-31 5:59 AM
I was going to write. But I don't receive anything. Is there a way to send packet to board's usart (for example: length of packet)?
2013-07-31 7:40 AM
I resolve it, but I don't understand. I changed GPIOC11 fromGPIO_Mode_IN toGPIO_Mode_AF and IRQ receive:
from if (USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) to
if (USART_GetFlagStatus(USART3, USART_FLAG_RXNE) != RESET)
what's the difference between
USART_GetITStatus and
USART_GetFlagStatus?
2013-07-31 7:55 AM
Yes, for F2/F4 designs the peripheral pins need to be in AF Mode.
If you want to send/receive multiple bytes you'll need to create some buffering, my preference is for ring/fifo buffers handled under interrupt. The USART has flags in in status register reflecting the state of internal registers and buffers, there is a secondary set of flags related to interrupt enabling, and status. These are covered in the Reference Manual for the parts.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.