STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Software vs Hardware resets

Posted on August 05, 2013 at 18:16 I have an application that is working fine when I have a hardware reset (pulling NRST low) but when it is power cycled, or has a software reset (NVIC_SystemReset();) It gets hung up on the following functions: ...

berge472 by Associate II
  • 3321 Views
  • 2 replies
  • 0 kudos

DfuSe Demo does not seem to upload DFU files to processtor

Posted on March 15, 2013 at 17:50I have installed DfuSe Demo (v3.0.0) . On connecting a STM3200G-EVAL board & setting the boot options & then pressing reset, the program says I am in DFU mode and gives the Vendor Id 0483 and the Product ID DF11 and ...

0690X000006053xQAA.png
rmhicks by Associate
  • 1806 Views
  • 4 replies
  • 0 kudos

What is the difference between Channels and Streams?

Posted on August 05, 2013 at 15:02Hello, I am a new starter of STM32. I'm quite confused by the concepts of Channels and Streams while dealing with DMA. What is the difference between them? Any comments will be appreciated, cheers. #dma-stm32f4di...

ran2 by Associate III
  • 5458 Views
  • 4 replies
  • 1 kudos

Zero Jitter ISR for STM32F051

Posted on August 05, 2013 at 17:00Hi,On STM32F051 I am trying to implement zero jitter interrupt servce routine for TIM6. I understand in Cortex-M0 architecture, there is a way to set higher IRQ latency to achieve zero jitter. I am not able to locat...

dr by Associate
  • 970 Views
  • 1 replies
  • 0 kudos

STM32 USART3

Posted on August 02, 2013 at 06:30Hello All, I am using USART3 in Half duplex mode for 1 wire protocol. The reset pulse of the one wire protocol has to be sent at 9600 and data exchnage at 115200. The problem I am facing here is BRR register doesnt ...

problem on watchdog

Posted on August 05, 2013 at 14:51Hi everbody,I'm using a ST32F205VE. On my board, I'm using the internal watchdog of the microcontroller and an external watchdog (MCP1318T).During normal operation, the �c sends square pulses every 0.5s to the exter...

SPI configuration

Posted on July 26, 2013 at 08:00hello i have configure the SPI1 in the stm32F0 for a data acquisition from a sensor. I marked that the processor always enter in the RXNE interrupt  despite there is no  data in the MISO pin.    /* SPI1 Periph clock e...

Cesar cfg by Associate II
  • 1897 Views
  • 4 replies
  • 0 kudos

STM32 SPI Hardware CS Generation

Posted on December 17, 2012 at 16:00 I'm working with the STM32F407VG chip (both on the STM32F4Discovery board and a custom board) and having trouble with the SPI port chip select in master mode. The following is the minimal code to demonstrate ...

jhaines by Associate
  • 4126 Views
  • 5 replies
  • 0 kudos

problem with long response in SDIO.

Posted on August 04, 2013 at 10:32Hullo guys , i have my own SD library working fine , but the problem is that i can not detect the card capacity because according to the datasheet (of STM32F2XX) ...... SD cards do not return long responses . so whe...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.