2013-08-01 9:30 PM
Hello All,
I am using USART3 in Half duplex mode for 1 wire protocol. The reset pulse of the one wire protocol has to be sent at 9600 and data exchnage at 115200. The problem I am facing here is BRR register doesnt get updated with baud rates. HSE_VALUE is 8Mhz SYSCLK(Hz) |64000000 APB1 prescalar is 16 I am not getting the proper baud rate and hence i get just 0 from 1 wire slave. Could anyone pls help in resolving this issue . Thanks #usart-rcc #stm322013-08-02 1:45 AM
Here's an example;
http://we.easyelectronics.ru/STM32/stm32-1-wire-dma.html2013-08-02 6:46 AM
Not being able to change a register is often an indication hat the peripheral clock is not enabled. Make sure you turn ont he USART3 clock in the RCC.
Jack Peacock2013-08-04 10:46 PM
Thanks Jack for the reply.
I have Enabled the USART 3 clock which is APB1 and 16Mhz. But still i cannot find any chnages. RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3,ENABLE); The other USART1 which uses APB2 (4Mhz ) is working propely Any suggestions?? Thanks2013-08-05 7:21 AM
Any suggestions??
Sorry, not guessing. Show enough code that someone could reasonably provide some suggestions. State the processor being used here, and the reason for the APB2 to be clocked slower than APB1, not sure it won't work but does seem to be backward. APB2 should generally be the same or faster than APB1.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.