STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How the image send from camera to computer? Help me

Posted on August 12, 2013 at 13:21I have a project with OV7670 with stm32f4-discovery. My OV7670 has 16 pins and without fifo. I want to the get one image with camera and I have to send this image to computer. But I don't have any idea. Help me. My ...

muhammet by Associate II
  • 3964 Views
  • 8 replies
  • 0 kudos

Help me USART STM32F4

Posted on August 09, 2013 at 18:34What is wrong. it isn't show data in terminal, ********************************************************************** &sharpinclude <stm32f4xx.h> &sharpinclude <stm32f4xx_rcc.h> &sharpinclude <stm32f4xx_gpio.h> &sh...

TIM channels and pin, I need a clarification!

Posted on October 11, 2012 at 13:33 TIM channels and pin, I need a clarification! I'm looking at the example TIM_PWM_Output (STM32F4-Discovery_FW_V1.1.0) /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_...

orn by Associate II
  • 1986 Views
  • 2 replies
  • 0 kudos

I2S standards - strange values

Posted on August 12, 2013 at 20:14 Hi I am using the I2S bus to transfer audio samples from an audio codec module to the microprocessor. There are several standards for I2S like Phillips, MSB, LSB or PCM. With the Phillips standard, every...

Smt32w SampleMac 2 library - simplest project

Posted on August 14, 2013 at 10:59I try to make minimal progect from exaples, but they use EVAL librarys for demo board. Can i make minimal progect use SimpleMac library without HAL library and EVAL library? #smt32w-samplemac

ADC regular channels vs injected channels

Posted on August 12, 2013 at 13:52Hello,Can somebody kindly explain the difference/ different usage scenarios of ADC regular channels and injected channels?As per available documentation, it is mentioned injected channels are intended, when the conv...

SysTick_Handler suspended during other interrupts

Posted on August 13, 2013 at 17:12Hello Allm I am prototyping with the STM32 F3 Discovery board and using the ST standard peripheral library.  I am also using some example code that contains a function - Delay() - which uses the SysTick_Handler to d...

STM32F37x SRAM size

Posted on August 13, 2013 at 14:23Hi, I have a simple question regarding internal SRAM size of STM32F373Rx processor. Datasheet (rev.3, table 2 on page 10) specifies SRAM size of 24kB for 128kB Flash units,but I can read and write up to 32kB of SRAM...

bpacan by Associate II
  • 1725 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.