2013-08-12 4:21 AM
I have a project with OV7670 with stm32f4-discovery. My OV7670 has 16 pins and without fifo. I want to the get one image with camera and I have to send this image to computer. But I don't have any idea. Help me.
My code:/**
****************************************************************************** * @file main.c * @author MCD Application Team * @version V1.0.0 * @date 18-April-2011 * @brief Main program body ****************************************************************************** * @attention * * THE PRESENT FIRMWARE WHICH IS FOR GUIDANCE ONLY AIMS AT PROVIDING CUSTOMERS * WITH CODING INFORMATION REGARDING THEIR PRODUCTS IN ORDER FOR THEM TO SAVE * TIME. AS A RESULT, STMICROELECTRONICS SHALL NOT BE HELD LIABLE FOR ANY * DIRECT, INDIRECT OR CONSEQUENTIAL DAMAGES WITH RESPECT TO ANY CLAIMS ARISING * FROM THE CONTENT OF SUCH FIRMWARE AND/OR THE USE MADE BY CUSTOMERS OF THE * CODING INFORMATION CONTAINED HEREIN IN CONNECTION WITH THEIR PRODUCTS. * * <h2><center>© COPYRIGHT 2011 STMicroelectronics</center></h2> ****************************************************************************** *//* Includes ------------------------------------------------------------------*/
&sharpinclude ''stm32f4xx.h'' &sharpinclude ''usart.h'' &sharpinclude ''LCD/LCD.h'' &sharpinclude ''camera/dcmi_OV7670.h''/** @addtogroup STM32F2xx_StdPeriph_Examples
* @{ *//** @addtogroup IOToggle
* @{ */ void LCD_CS_ResetBits(void); void Delay(__IO uint32_t nTime); void TimingDelay_Decrement(void); static __IO uint32_t TimingDelay;uint32_t fps=0;
uint32_t disfps=0; uint32_t fpsbuff[5]; /** * @brief Main program * @param None * @retval None */ int main(void) { OV7670_IDTypeDef OV7670ID; RCC_ClocksTypeDef SYS_Clocks; uint8_t i=0; /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f2xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f2xx.c file */ if (SysTick_Config(SystemCoreClock / 1000)) { /* Capture error */ while (1); } RCC_GetClocksFreq(&SYS_Clocks);USART_Configuration();
//USART_NVIC_Config();printf(''\r\nSYSCLK:%dM\r\n'',SYS_Clocks.SYSCLK_Frequency/1000000);
printf(''HCLK:%dM\r\n'',SYS_Clocks.HCLK_Frequency/1000000); printf(''PCLK1:%dM\r\n'',SYS_Clocks.PCLK1_Frequency/1000000); printf(''PCLK2:%dM\r\n'',SYS_Clocks.PCLK2_Frequency/1000000);LCD_Initializtion();
LCD_Clear(Red); DCMI_OV7670_Init(); /*Set LCD direction*/ LCD_WriteReg(0x0011,0x6068); LCD_SetCursor(0,0); Prepare_Write_RAM(); /* Start Image capture and Display on the LCD *****************************/ /* Enable DMA transfer */ DMA_Cmd(DMA2_Stream1, ENABLE);/* Enable DCMI interface */
DCMI_Cmd(ENABLE);/* Start Image capture */
DCMI_CaptureCmd(ENABLE); while (1) { Delay(1000); fpsbuff[i]=fps; fps=0; i++; if(i==5) { disfps=(fpsbuff[0]+fpsbuff[1]+fpsbuff[2]+fpsbuff[3]+fpsbuff[4])/5; printf(''FPS:%d\r\n'',disfps); i=0; } } }void Delay(__IO uint32_t nTime)
{ TimingDelay = nTime;while(TimingDelay != 0)
{} }void TimingDelay_Decrement(void)
{ if (TimingDelay != 0x00) { TimingDelay--; } }void LCD_CS_ResetBits(void)
{ GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);//LCD_CS PD7
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOD, &GPIO_InitStructure);GPIO_ResetBits(GPIOD , GPIO_Pin_7); //CS=0;
}&sharpifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) *//* Infinite loop */
while (1) {}
} &sharpendif/**
* @} *//**
* @} *//******************* (C) COPYRIGHT 2011 STMicroelectronics *****END OF FILE****/
#best-forum-software-ever2013-08-12 7:13 AM
You've got an LCD attached?
Seems to be some F2 code/comments mixed in. Can you send the data via the serial port, or USB perhaps?[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/How%20the%20image%20send%20from%20camera%20to%20computer%20Help%20me&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=7]Related? If this is home work or course project work, you should discuss with your instructor2013-08-13 1:11 AM
Thank you for answer. The problem is that I don't know how can I get data from camera. After that I want to send this data to computer. Finally I will use interface to see image.
2013-08-13 9:42 AM
What does the documentation say?
Have you reviewed any DCMI examples, or ones for boards that have camera attachments? STM32F4xx_DSP_StdPeriph_Lib_V1.1.0\Project\STM32F4xx_StdPeriph_Examples\DCMI\DCMI_CameraExample2013-08-14 6:45 AM
I get the data from DMA and I send this data to array. Last of this I send all of data to computer via usart. But I see only ''0''.
DMA_DeInit(DMA2_Stream1); DMA_InitStructure.DMA_Channel = DMA_Channel_1; DMA_InitStructure.DMA_PeripheralBaseAddr = DCMI_DR_ADDRESS; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t) buffer_A; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = sizeof(buffer_A); DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream1, &DMA_InitStructure); for(i=0 ; i<640*16 ; i=i+2) { printf(''%d'',buffer_A[i]); }2013-08-14 7:24 AM
The size is in 32-bit words, not bytes, you'll need to scale the sizeof()
Does the buffer have visible content in the debugger? Is any data getting transferred via DMA from the DCMI? Try putting a fill pattern in there if you are not sure.2013-08-14 7:24 AM
wait until the DMA is finished?
2013-08-14 7:25 AM
Funny. I get a double post when I get a web page error
2013-08-14 7:44 AM
Funny. I get a double post when I get a web page error
One of the errors occurs when it tries to display your new post. Hit back (some browsers retain your edit, FireFox), or open the forum in another tab and confirm if the post stuck.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.