2012-08-30 5:57 PM
After reviewing the (very informative) application note on ''STM32's ADC modes
and their applications'', which is located at the site below, I was curious where I can find the numerous examples which are referenced in the note, and which allegedly are attached to it. Examples are:- Dual_FastInterleaved, page 10- Dual_AlternateTrigger, page 13- Dual_Combined_Reg_Inj_Sumultaneous, page 14, ... etc.Thanks for your help,JJ2012-08-30 6:23 PM
A lot of the examples have percolated into the standard peripheral library example files.
Are you looking for the STM32F1xx parts or the more recent F2 or F4?2012-08-30 8:24 PM
After a bit of Googling I have this
http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/FIRMWARE/an3116.zip
2012-09-06 2:22 PM
Muchos gracias! Exactly what I was looking for (exact version not so important, I just wanted to see the implementation as guidance).
Thanks again.2013-08-14 4:41 AM
Hello,
At the moment I could not find sample Firmware in the given location, instead I came across those in the following location.http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF257864
May be ST have shifted the location.Anyway thought it would be helpful to share this location, for the sake of someone else searching for the samples.:)Thanks.-Anuradha.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.