STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C3 interrupt not working

Posted on August 29, 2013 at 15:54 Hi all, I have some problems with I2C3 interrupts, I have enabled the interrupt but the handler interrupt never executes. Here is the interrupt configuration: NVIC_InitTypeDef NVIC_InitStru...

edgar by Associate II
  • 796 Views
  • 0 replies
  • 0 kudos

File System

Posted on August 24, 2013 at 13:10I am implementing file system for stm32f407vg controller. I am getting problem in implementing directory next function. can any one help me ?

srinivas by Associate
  • 1555 Views
  • 3 replies
  • 0 kudos

Writing on USB-Memory

Posted on April 12, 2013 at 07:58Hello, i have a little problem. I have adaptet the stm_Host_MSC example on my board. I use the USB_HS_Core with the internal FS-phy. I can communicate and wirte on my usb-stick. my question mow is: What i have to do,...

STM32L152 LSERDY

Posted on August 28, 2013 at 08:58Hi, I have a batch of STM32's which use the LSE.  On all of the device LSE starts normally(i.e. you can see it oscilate with a scope).  However, on a few of the devices LSERDY never aserts to indicate that the clock...

allison by Associate
  • 1773 Views
  • 3 replies
  • 0 kudos

STM32 Timers + Interruptions - Error

Posted on August 28, 2013 at 12:46 Hi, I set an interruption handler for a timer. Each time it calls the handler I change the state of a IO. But I'm getting problems for frequency above 80kHz. If I set the period to: TIM_TimeBas...

0690X00000604slQAA.png 0690X000006050oQAA.png
ee06091 by Associate III
  • 1374 Views
  • 1 replies
  • 0 kudos

Need information about ADC's external impedance

Posted on August 28, 2013 at 11:17Hi everyones,In the datasheet for STM32F407xx, in the electrical characteristics part (12-bit ADC characteristics), they deal with the Rain value. they define it like that : used to determine the maximum external im...

STM32L-Discovery SPI to ADS1118

Posted on August 28, 2013 at 08:41The original post was too long to process during our migration. Please click on the attachment to read the original post.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.