STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32 Encoder interface

Posted on July 12, 2011 at 11:20Nid help in Stm32 Encoder Interface, to turn the motor in clockwise and anti-clockwise direction. Thanks  #encoder-interface #stm32f0-discovery

Making reserved bits at reset value

Posted on August 31, 2013 at 09:29In many of registers of STM32F205 it is mentioned that reserved bits should be kept ar reset state.Is it sure that reading reserved bits always return its reset value or its undefined. If it is undefined then have t...

programming STM32F0 over UART

Posted on July 08, 2013 at 14:53Hi guys, i need to program a stm32f0 mcu using a serial cable.At this moment i'm using an external St-link device.Can i use only a serial cable without st-link (e.g. over hyper terminal)? #uart

pietro2 by Associate II
  • 5808 Views
  • 10 replies
  • 0 kudos

Simple Menu example for touch screen

Posted on August 30, 2013 at 16:07 Good afternoon all, I am experimenting with the STM32F4Discovery boards and till now I have managed to interface with pin PC0 by connecting a pot and showing the value of its resistance on the LCD touch screen ...

0690X0000060MnsQAE.gif
philip by Associate
  • 880 Views
  • 0 replies
  • 0 kudos

Flash Loader Demonstrator v2.6.0 bug: RTS line control issue

Posted on August 30, 2013 at 08:34I am using STMFlashLoader.exe on Windows 7 (64bit).RTS Output control in Command line version doesn't work.DTR control works fine.To the STMicroelectronics software designers.  This is obviously bug in theSTMFlashLo...

vvvalka by Associate
  • 693 Views
  • 0 replies
  • 0 kudos

STM32 Timers - Help with TIM_Period

Posted on August 28, 2013 at 12:14Hi,I'm studying the timers on STM32F100 using a STM32VLDISCOVERY board.Per example:  TIM_TimeBaseStructure.TIM_Prescaler = SystemCoreClock/1000 - 1; TIM_TimeBaseStructure.TIM_Period = 1;Will set the count frequency ...

ee06091 by Associate III
  • 1991 Views
  • 3 replies
  • 0 kudos

USB virtual com port for stm32f3discovery

Posted on February 15, 2013 at 19:33Hi,I plan to transfer the gyroscope value to PC through USB virtual com port. So I downloaded the latest version for the USB full speed device library for stm32(version 4.0). However, the projects, specifically th...

vsaaket8 by Associate II
  • 2226 Views
  • 5 replies
  • 0 kudos

Overwriting written flash memory with 0xFFFFFFFF on STM32L

Posted on August 27, 2013 at 20:48I need a reliably method of overwriting flash memory on a STM32L device (STM32L152CB). On the other STM32F series, this was easy, as I could write zeros on top of previously written flash memory contents reliably. T...

mlakata by Associate II
  • 6310 Views
  • 10 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.