STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 I2C issues

Posted on September 01, 2013 at 18:26Hello, I am trying to get the I2C bus to run with the MMA8452 accelerometer, but it just wont. I can generate a start condition but nothing else. I'm watching the bus lines with a scope/logic analyzer and I can s...

totally by Associate II
  • 1833 Views
  • 3 replies
  • 0 kudos

Stm32f4 ADC exemple

Posted on August 31, 2013 at 19:50hello i tried ST's adc exemple and i got weird values of my variable while debugging , for exemple i got 30 for 2.0 v and -1000 for 2.5 v , so anyone have a working code with no weird things? and thnx :)

help - F103 window watchdog

Posted on August 31, 2013 at 21:45 hello dear forum, I am trying to setup window watchdog on F103 I want wwdg to be reset in a window of 8 - 12 milisecond I set wwdg prescaler to 2 so wwdg timer is counting every 0.227 microsecon...

STM32L151 Signals generator with time shift/delay

Posted on August 28, 2013 at 16:10Hi,I'm trying to generate 3 signal using TIM3&TIM4.the first signal run at 8MHz, DutyCycle 50%, the second signal should run every odd cycles of the first signal and the third should run every even cycles of the fir...

0690X000006051DQAQ.png
tamir by Associate
  • 1742 Views
  • 3 replies
  • 0 kudos

Exiting STOP mode on USART character

Posted on August 30, 2013 at 14:27 Hi, I have a bit of an issue - I'm trying to put an STM32 into STOP mode, but to have it wake up when a character is sent over the USART (and to receive that character). My code is just: // .....

gw by Associate II
  • 1456 Views
  • 3 replies
  • 0 kudos

minimum HCLOK for USB OTG FS

Posted on September 01, 2013 at 09:24I use today HCLK of 120Mhz taken from the systemclk of 120Mhz (prescale by 1), and active USB OTG FS no problem. To save power I want to go as much as possible low with the freq, when not during fast operations, ...

Barbie by Associate II
  • 753 Views
  • 0 replies
  • 0 kudos

I2C on STM32F4 gets stuck while checking EV6 flag

Posted on May 26, 2012 at 10:14 Hi guys, I'm working on a STM32F4 Discovery board and trying send over I2C. Therefore I'm using the functions from the Standard Peripheral Library. Unfortunately the device stucks after sending the address ...

return address of isr

Posted on August 31, 2013 at 20:31hi i am working on stm32f4. i am having a small programming issue, while my code is executing, ISR comes, i want to change the return address of ISR, i.e it does not goes back from where the processor left the code....

bilal by Associate II
  • 1097 Views
  • 1 replies
  • 0 kudos

JavaScript interpreter on STM32 Discovery boards

Posted on February 13, 2013 at 11:34Just to say about a project I've been working on - it's a JavaScript interpreter for the STM32 called Espruino (http://www.espruino.com)It's available for the STM32VL, STM32F3 and STM32F4 boards - as well as some ...

gw by Associate II
  • 829 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.