2013-09-01 12:24 AM
I use today HCLK of 120Mhz taken from the systemclk of 120Mhz (prescale by 1), and active USB OTG FS no problem.
To save power I want to go as much as possible low with the freq, when not during fast operations, and go back to 120Mhz for fast operations. I read in the manual that the HCLK should be more then 14.2Mhz for USB OTG FS to work. So I try to go to 15Mhz by prescale the systemclk by 8 (from 120Mhz). I also read that I need to stratch USB response time to IN tokens so I do so and set it to 0x0F. It is writen like this:/* HCLK = SYSCLK / 8*/
RCC->CFGR &= ~(RCC_CFGR_HPRE); // clear AHB prescaler RCC->CFGR |= RCC_CFGR_HPRE_DIV8; // get Down not lower then 15Mhz for UART BAUD RATE but also for USB FS OTG proper operation /* keep PCLK2 stay at same original freq */ RCC->CFGR &= ~(RCC_CFGR_PPRE2); RCC->CFGR |= RCC_CFGR_PPRE2_DIV1; /* keep PCLK1 stay at same original freq */ RCC->CFGR &= ~(RCC_CFGR_PPRE1); RCC->CFGR |= RCC_CFGR_PPRE1_DIV1; /* Setup SysTick Timer for 10ms interrupts according new HCLK */ if (SysTick_Config((SystemCoreClock/8) / 100)) { /* Capture error */ while (1); } USB_OTG_dev.regs.GREGS->GUSBCFG &= ~(0xF << 10); USB_OTG_dev.regs.GREGS->GUSBCFG |= 0xF <<10; I also check what is the new freq by operating RCC_GetClocksFreq(&RCC_ClockFreq); and see I get HCLK 15Mhz . and I get the right setting in the USB stratch time. But after doing so the USB not recognize on the PC. I try to do the freq adjustment before and after USB init but not help. When I pick HCLK of 30Mhz it is work O.K. What could be the reason? Bar.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.