STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Switch JTAG to SWD port on STM32L4

Hi,I'm working on an STM32L4R5ZIT6 mcu and I'm facing with the problem of switching the JTAG port to SWD without the use of a debugger (ST-Link or similar); reading the "Arm Debug Interface" document I found the way to make the switch and in fact, us...

DUrbano by Associate III
  • 1910 Views
  • 2 replies
  • 1 kudos

Resolved! J1939 support in STM32G491KCU6

Hi Expert, We are planning to use J1939 protocol for vehicle communication. We would like to clear few queries regarding this. Is J1939 CAN stack openly available? If no, do we need to purchase it? Is sample application available for communication us...

ssuresh by Associate II
  • 1617 Views
  • 1 replies
  • 1 kudos

STM32H7S3L8 PSSI with DMA

Hello everyone, I am trying to use the PSSI peripheral with DMA on my nucleo-H7S3L8, I am new to this GPDMA so at first i tried using the standard request mode and i got it working but it only receives once and stops do i need to manually enable it a...

Faisal129 by Associate II
  • 1933 Views
  • 2 replies
  • 0 kudos

ESD and MCU freezing

Hi everyone,we're using the STM34F407ZG microcontroller in our BMS board.We have some issue during contact 8kV ESD applied in some screws above the boards. The ESD are applyed on all the screws but the problematic one are just 3 screws, the closest s...

Lucast by Associate II
  • 4711 Views
  • 6 replies
  • 4 kudos

Resolved! MCU Errata vs HAL, LL

Hi there,this is an general question.Every serious engineer walks thru errata document as it gets published.So do I now.Do I have to review every HAL / LL function which may coincide with erratic behaviour?Is proposed in errata workaround already imp...

DrDro by Associate III
  • 1614 Views
  • 1 replies
  • 3 kudos

Resolved! GPIO Read interact with GND or VCC

Hi,I use STM32F103C8T6 a GPIO input pin to read a high or low signal from another GPIO output pin, and connect a 3Mohm resistor between two pins, and I notice touching GND with hand will influence the signal status, than I measure the resistance betw...

ULOK by Associate II
  • 3467 Views
  • 5 replies
  • 3 kudos

Resolved! Timer Input Capture - Setting frequency - STM32F051

Hi,I am trying to configure an input capture on my STM32F051R8Tx. It works fine, I am supplying an external signal via a signal generator and my code measures exactly T=4ms pulses - which I expect. In my case, I am sampling with 24MHz, so the measure...

LT.1 by Associate II
  • 2237 Views
  • 2 replies
  • 2 kudos

Resolved! STM32H755 Supply connection

Hello,I'm working on project with STM32H755ZIT6. Currently I use Nucleo Board, but I designed prototype board, but the board don't work. I supose that problem is caused by wrong connection for supply.I use +3.3V from DC/DC connerter for suplly. Can s...

koyocik by Associate III
  • 9714 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.