STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem stm32f101x UART4

Posted on November 05, 2013 at 14:57The original post was too long to process during our migration. Please click on the attachment to read the original post.

tiaandpz by Associate II
  • 3608 Views
  • 6 replies
  • 0 kudos

STM32F102CBT6 Timer 4 question

Posted on November 05, 2013 at 09:51Hi all. I'm new to ST micro's so excuse me if this is a dumb question. I'm working on a project using the above micro. I'm using Atollic as my ide. I'm trying to get timer 4 working. The code compiles , but in the...

Rob1 by Associate II
  • 1749 Views
  • 3 replies
  • 0 kudos

STM32F407 pll clock configuration

Posted on October 31, 2013 at 17:31Hi,i'm new user... i'm studying the microcontroller in the subject and i've read that usart 1 and 6 are able to work up to maximum baud-rate of 10.5Mbps. Is it right?Ok, now for my application i need to configure t...

frantic by Associate II
  • 4149 Views
  • 8 replies
  • 0 kudos

STM32 orcad symbol

Posted on November 04, 2013 at 10:20is available for download the orcad symbol for the microcontrollers STM32F407VG and STM32F103C8T6?Thanks

frantic by Associate II
  • 1556 Views
  • 1 replies
  • 0 kudos

Set FLASH level protection from Level 1 to Level 0

Posted on November 06, 2013 at 12:23I am programming the STM32F051x6 micro with the IAR Embedded Workbench IDE and the ST-LINK. I erased the Flash option bytes and now I can not load my application code into the micro with the ST-LINK because the Fl...

ecatala by Associate II
  • 1651 Views
  • 2 replies
  • 0 kudos

STM32_USB-Host-Device_Lib_V2.1.0 Not available?

Posted on November 03, 2013 at 03:53I would like to download STM32_USB-Host-Device_Lib_V2.1.0 (STSW-STM32046), but there is no download link on the page: http://www.st.com/web/en/catalog/tools/PF257882 Is it available elsewhere?

wrlear by Associate
  • 1667 Views
  • 3 replies
  • 0 kudos

i2c is not working for stm32f051

Posted on November 05, 2013 at 16:51Hello everybody, I have an application for the STM32f051 wich has a i2c device connected I have configured and initialized the i2c, however when I send some data both SDA and SDI lines are staying 'high', I don't ...

evert2 by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos

how to sync two stm32 chips' DMA section?

Posted on November 04, 2013 at 00:36i have three stm32f1x chips working with one  oscillator on the same pcb board. it works well. the three chips, let's say A, B, C, A as master chip, B and C as slave chips. now i need to achieve very high speed co...

wonss by Associate
  • 2581 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.