STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to recover data from SD?

Posted on November 07, 2013 at 12:14Hello everyone,I'm writing data to SD for a few seconds/minutes. If I disconnect the board while recording, when I look at the file with windows, it shows the file with an extension of 0Kb. How can I fix the file ...

Changing Timer Triggers on the Fly...

Posted on November 07, 2013 at 18:17I have designed a variable pulse generator using the STM32F4 and using 7 timers which outputs on three pins, using AF pin couplings to TIM1/TIM8/TIM9(all operated in OPM mode) because I wanted the 6ns resolution p...

jason2 by Associate II
  • 991 Views
  • 1 replies
  • 0 kudos

Multi DMA channel configuration

Posted on November 06, 2013 at 23:06Hi, Last time, I programed multi channel ADC with channel0 of DMA2_stream0. And now I try to add one more channel for USART with DMA2_stream0. I know each DMA stream has maximum 8 channel and they share DMA_SxCR...

STM32F427II (UBGA176) can not program

Posted on November 06, 2013 at 22:39Hi Everyone,I have just finished a project with the MCU STM32F427II but I can not program it. I use the ST-LINK v2 programmer with a 4 wire (SWD).I have check all the connection and I found that the pin (bypass_re...

dombog by Associate
  • 2018 Views
  • 3 replies
  • 0 kudos

Problem with Flash Loader Demonstrator and STM32F407ZG

Posted on June 11, 2013 at 13:02Hi,I'm trying to use FLD v2.6.0 with STM32F407ZG rev Z. No problem to connect, uploading an image written by SWD works most of the time, erasing and downloading gives mixed error messages such as for example that eras...

STM32F2xx USART 9 Databit, 1 Start bit, 2 stop bit, parity odd

Posted on November 06, 2013 at 09:34Hello, i'm trying to get a USART connection to a device with the parameters:  USART 9600 Baud, 9 (real)Databits, 1 Start bit, 2 stop bits, parity odd. I configured my USART like this: USART_InitStructure.USART_Bau...

f2 by Associate II
  • 3665 Views
  • 9 replies
  • 0 kudos

NVIC_EnableIRQ() causes Hardfault

Posted on November 05, 2013 at 19:34Hello,I'm using a STM32-discovery Board equiped with a STM32F100RB. Till now all I'm trying to do is to call the Interrupt-Handler of TIM3. But when calling NVIC_EnableIRQ(TIM2_IRQn) the programm is always running...

klaas by Associate
  • 3796 Views
  • 5 replies
  • 0 kudos

STM324x9I-EVAL Demo Software

Posted on November 06, 2013 at 17:45I have just got hold of an STM324x9I-EVAL board as a base to develop a platform for new products. I am unable though to locate a version of the STM32F2-F4_Demonstration_Builder which supports this board. In fact I...

simon23 by Associate
  • 1291 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.