2013-10-31 9:31 AM
Hi,
i'm new user... i'm studying the microcontroller in the subject and i've read that usart 1 and 6 are able to work up to maximum baud-rate of 10.5Mbps. Is it right?Ok, now for my application i need to configure the baud rate of these two usart to 10Mbps.How should i configure PLL registers in order to meet my needs?Could you help me please?Is there any issues to be considered in making what i want (DMA, Interrupts and so on)?Thanks2013-10-31 9:51 AM
For 10 Mbps (10,000,000 exact) I'd opt for running the core at 160 MHz (PLL_N 320), APB1 @ 40 MHz, APB2 @ 80 MHz
You'd need to run the USART in 8x oversample mode, I'm not sure of the practicality of running at 10 Mbps, I'd be using a synchronous interface at those rates. Have fun.2013-11-04 2:42 AM
Ok thank you...
I have another question...is it possible to perform the conversion from ethernet to 10Mbps usart and vice versa? Are there any issues to be considered in this kind of operation?If possible could you give some information about that?Thanks again2013-11-04 7:57 AM
I'm sure it's ''possible'' but you'd have to pay me to demonstrate it's impracticality.
Explain better the ''real'' problem you're trying to solve.2013-11-05 8:01 AM
http://www.at91.com/forum/viewtopic.php/t%2c21983/
2013-11-06 12:55 AM
I'm considering different microcontrollers for a project that I have to develop. In the end I chose stm32.
what's the problem?2013-11-06 5:02 AM
what's the problem?
Apparently one of a lack of experience/appreciation for the issues with async signalling at 10 Mbps. This is compounded by your inability to clearly explain what the ''real'' problem is that you're trying to solve, and instead focusing on a flawed interface choice with no supporting information. If you can't explain, perhaps a diagram would help?2013-11-06 6:02 AM
no problems for now i'm only looking for information...
2013-11-06 6:23 AM
no problems for now i'm only looking for information...
So you picked a 10 Mbps USART out of the air, with no particular driver? Perhaps you should sit down with your project supervisor, and formulate a system diagram for what it is you're trying to achieve.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.