STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to achieve max. accuracy for static timing event

Posted on November 17, 2013 at 00:24Hello :)I want a timer to execute ISR all 4 ms but for academic reasons (interest) I want it as accurate as possible. So I chose TIM_Prescaler = 0 and TIM_ClockDivision = 0.Is there anything else that could increa...

STM32VL Discovery -> Strange Voltages

Posted on November 16, 2013 at 19:21So far from the help here (mainly clive1) I got my timers running, GPIO initialized and some demo code running.  The device I am trying to control is not recognizing the data I am trying to send to it so I dug a l...

mistake in stm32f4xx.h

Posted on November 16, 2013 at 17:31to be migrated, sourceId: 35463:697285D7-A9CA-445D-B16C-F23BF0E3B1A3 #stm32f4

SYSCLK

Posted on November 16, 2013 at 17:00I read in system_stm32f4xx.c that after reset, sysclk is 168MHz. I want to creat a function delay 1s.void Delay(void) { uint32_t i; for(i=0; i<0xA037A00; ++i)   // A037A00 = 168.000.000 { }   }.Who can explain fo...

41003160 by Associate II
  • 1660 Views
  • 3 replies
  • 0 kudos

Timer 5 never counts from zero

Posted on November 16, 2013 at 05:57 #define SYS_CLK 24000000 /* in this example we use SPEED_HIGH = 24 MHz */ #define DELAY_TIM_FREQUENCY 1000000 /* = 1MHZ -> timer runs in microseconds */ /* Enable timer clock - use TIMER5 */ RCC_APB1PeriphC...

stm32f103rb NSS

Posted on November 15, 2013 at 02:58hello,I have a problem about the stm32f103rb. According to the RM0008  reference manual downloaded in your website, I find the description of  slave select(NSS) pin management. So the NSS signal can be driven high...

wwtzh2013 by Associate II
  • 1877 Views
  • 3 replies
  • 0 kudos

USART communicatoin with DMA

Posted on November 15, 2013 at 19:30The original post was too long to process during our migration. Please click on the attachment to read the original post.

STM32F4 FreeRTOS and us accuracy delay

Posted on November 13, 2013 at 13:07Hi everyone, I'm currently working on a musical (using midi) project on which i need very precise delay in order to synchronise with other instruments. This delay should be able to be accurate at 1 microsecond. Fo...

benoit2 by Associate II
  • 2679 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.