STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DAC & ADC speed help

Posted on November 12, 2013 at 15:54 Hello, I'm coding a real time system based on STM32F427 requiring a lot of ressources and using almost all peripherials (ADC, DAC, SPI, I2aC, USART, USB, SDIO). This is why I want to reduce the ressou...

SPI slave using DMA on STM32F405RG

Posted on November 15, 2013 at 10:31I am working on the SPI communication between PC and STM32F405RG MCU. FTDI chip FT232H serves as a bridge between PC and MCU (USB to SPI converter). FTDI is set to be SPI master and MCU is slave. I am using DMA tr...

milos by Associate
  • 924 Views
  • 0 replies
  • 0 kudos

Very simple SPI code doesn't do anything

Posted on November 13, 2013 at 01:03Hello experts,I'm trying to get SPI with DMA running on my STM32F3board. So I wrote this code after a tutorial and the StdPeriph Lib. To test the SPI parameters I wanted  to send a 16 bit value and watch on the bu...

f407 read/write flash error

Posted on November 13, 2013 at 11:03i use my own board and try to use SD card to update IAP when i try to erase/write flash the function always return ''flash_error_program''i checked flash->sr value is 0xC0, but i just follow the step with stm32f4_...

stm32f303 bootloader problem

Posted on November 13, 2013 at 23:43I can successfully load the code from stm32f407 processor to stm32f100 in my project by using f100's bootloader firmware and RS232 protocol. However, I used the same(similar) way to load the code to stm32f303 proc...

mli by Associate II
  • 4397 Views
  • 10 replies
  • 0 kudos

STM32F429 DISCO with ULINK2 debugger

Posted on November 13, 2013 at 21:16 Has anyone managed to connect a ULINK2 (or other JTAG debugger) to the STM32F429 Discovery using CN2, if so, how? Yes, I know the Disco comes with a ST LINK V2 interface, and that works just fine, for now. But, e...

STM32F4 - Discovery ADC Example Problem

Posted on November 14, 2013 at 14:57Hello everyone,I've been trying to discover the STM32F4-Discovery features and peripheral examples of its firmware package lately. I'm having trouble with the ADC-DMA example. Actually, I wanted to observe only co...

Starting with DSP - CHIBIOS

Posted on November 12, 2013 at 16:38Hi all, i would like to start programming some DSP application with my board (STM32FDISCOVERY) ,my software framework is Eclipse with GNU Tools Arm Embedded compilers with CHIBIOS / OPENOCD for debugging and progr...

pure 8-Bit SPI communication ?

Posted on November 14, 2013 at 10:34Hi, I am in trouble with 8-bit SPI communication. I did this:   SPI1->CR1 = (uint16_t)( SPI_CR1_MSTR | SPI_CR1_BR_0 | SPI_CR1_BR_1                           | SPI_CR1_SSI | SPI_CR1_SSM );   SPI1->CR2 = (uint16_t)(...

mmensch by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.