STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f051C6 PF6/7 AF for I2C

Posted on February 26, 2013 at 07:38Hello, I try to make I2C on PF6/7 on the STM32F051C6  (48 Pin device) working. To get what AF to use, Ref man points to the datasheet. But the datasheet is not clear to me, it has a AF Table for PortA and PortB an...

jgnoss by Associate III
  • 3678 Views
  • 5 replies
  • 0 kudos

SPI DMA data corruption

Posted on November 21, 2013 at 17:52Hi,I am using SPI2 with DMA1 on STM32F427 to communicate with an external processor. The problem is that when the data on MISO and MOSI pins (PB14 and PB15) are somehow corrupted i.e. the data comes out as shifted...

asecen89 by Associate II
  • 2179 Views
  • 4 replies
  • 0 kudos

STM32F373 SDADC Gain Error Issue

Posted on October 23, 2013 at 21:20Using the 3 channels of the SDADC in Single Ended Zero Reference Mode, Gain 1, with a SDREF at 2.5V.  Spec lists gain error of -2.4% to -3.1%, but our devices appear to have a positive gain error of approx +2.8%.  ...

Problem using NVIC_SetVectorTable on StmF3Discovery

Posted on November 22, 2013 at 00:44Hi there, I've got a problem here using NVIC_SetVectorTable(). I have attached my test programm, which is held very simple and does: - Init Leds&UserButton - make sure the ''new'' Vectortable is 0x200-aligned - Co...

STM32F303CB ==> RCC_ADCCLKConfig

Posted on November 21, 2013 at 16:23Hello, I have a problem with the RCC_ADCCLKConfig, I want to change the  ADC frequency and I followed the example from st.    /* Configure the ADC clock */   RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div64);     /* Enable...

stm32 I2s in slave mode Timing

Posted on November 22, 2013 at 11:57 The stm32 chip has a error for I2S in slave mode (stm32f40x Errata sheet 2.4.1). 2.4.1 In I2S slave mode, WS level must be set by the external master when enabling the I2S Description In slave mode, th...

Is there a way to reset SPI RxFifo?

Posted on November 21, 2013 at 15:25Hi, I would like to ask if there is a way to clear the FRLVL and RXNE bits in SPIx->SR in order to ignore everything that has been received before. I have some routines that only send data and other that will als...

mmensch by Associate II
  • 984 Views
  • 3 replies
  • 0 kudos

hard fault handler

Posted on August 04, 2013 at 01:47hi,i am working on stm32f407. i am experiencing hard fault handler. start:{}timer();while(!one_second_timer){ /*my code*/}goto start;and the code for timer is void timer(void){ uint16_t PrescalerValue = 0; TIM_Cmd(T...

bilal by Associate II
  • 1864 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.