STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC time shift in seconds for a day

Posted on November 23, 2013 at 14:58I have implemented RTC in STM32F107RB at 50Mhz operating frequency, it works good but the problem is shift in time about 5 to 6 seconds in a day. Is there any correction factor?  Here i have attached  RTC intialis...

aru by Associate II
  • 2209 Views
  • 2 replies
  • 0 kudos

FSMC driving LCD 8bit bus, but sending 2 bytes

Posted on April 17, 2013 at 08:26 Hi all, I have a ST7753S 8 bit bus, 8080 style, hooked up to STM32F103VE FSMC with config as below. However I find that there are 2 bytes being written every time I write a char. Is this how it works...

USB Audio volume taper

Posted on November 24, 2013 at 16:12Hello,I have implemented a USB microphone which uses OS default driver. I define the volume from 0x0C00 (MAX) to 0xE000 (MIN) correspond to +6dB...-24dB.Control in Windows,Linux works. However taper is the wrong w...

qweef by Associate
  • 806 Views
  • 0 replies
  • 0 kudos

How to use STM32F030F4

Posted on November 24, 2013 at 12:25Hello guys?      I have bought some STM32F030F4 chips ?but i donnot know how to program on it?I am confused of the Related firmware?So can someone tell me how to creat a new project using Keil-MDK without the give...

SPI MISO problem

Posted on November 23, 2013 at 23:09I know this is weird, but any help would be great. This is driving me nuts. I'm tyring to use A5, A6 and A7 as SPI for communication with a touchscreen controller. SCLK and MOSI work fine, but MISO (A6) works only...

SDIO clock doesn't seem to enable

Posted on November 22, 2013 at 17:19Hello community, I am trying to communicate a STM32F207 uC with a uSD card via the SDIO interface, what I am trying to do is to get the CID of the inserted uSD using CMD commands, and verify that both parts are co...

dmg0048 by Associate II
  • 1813 Views
  • 2 replies
  • 0 kudos

DCMI and DMA interrupts with phenomena

Posted on November 23, 2013 at 18:50 I'm now trying to receive an image from my OV9655 over the DCMI port and send it then to the pc. With low resolution (160x120 pixel) and saving the image in the ram it worked good. Now I want to geht higher r...

pa by Associate II
  • 2161 Views
  • 4 replies
  • 0 kudos

STM32 Interface with FSMC and DMA

Posted on March 21, 2012 at 12:56Hi, I have to read a 15 bit parallel data coming from a camera sensor and one bit as a request signal which tells whether the micrcontroller should initiate memory transfer or not. Does FSMC has any trigger signal ...

STM 32 F4 Discovery I2C Hanging Up

Posted on November 21, 2013 at 15:51Hi, I am having a problem with using the I2C on the STM 32 F4 discovery to read 3 DevanTech SRF-08 ultrasonic sensors, There was a previous post on this matter, but it was unresolved as far as I know, clive1 did i...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.