STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIMER2 INPUT CAPTURE

Posted on February 05, 2014 at 13:42Hi,Kit using : STM32Discovery Board(STM32F100 controller)I have implemented the input capture mechanism for Timer15 channel 1. In which I set triggering for both falling and rising edge.Now I am trying to port the...

sooraj by Associate
  • 1189 Views
  • 2 replies
  • 0 kudos

ST Link V2, SWO speed weirdness

Posted on February 13, 2014 at 05:38I have a bit of code to output some debug using SWOvoid swo_init(){ uint32_t SWOSpeed = SWO_SPEED; uint32_t SWOPrescaler = (SystemCoreClock / SWOSpeed) - 1; // SWOSpeed in Hz CoreDebug->DEMCR = CoreDebug_DEMCR_TRC...

usb otg host lib, where is NAK for bulk-IN?

Posted on February 13, 2014 at 05:31I am using a STM32F405RG as a USB host. I've implemented the ST USB Host library (version 2.1.0) in a way that supports multiple devices behind a hub. In order to seemingly support unlimited devices (as much as po...

Problem connecting to STM32F051 via STM32F0DISCOVERY

Posted on February 09, 2014 at 16:57Hi, I have a problem connecting to a STM32F051K6. I tried to use the Debugger on an STM32F0DISCOVERY-Board. It should be an ST-Link V2. Therefore I disconnected the Jumpers on CN2 and the Soldering bridges on SB19...

j_ by Associate II
  • 2725 Views
  • 4 replies
  • 0 kudos

STM32F0308-DISCOVERY I2C Configuration

Posted on February 12, 2014 at 20:22My original post *poof* gone..I am attempting to use I2C2, however Oscilliscope does not see any activity on either SCL or SDA. Using STM32F0308-Discovery. Obviously timing parameter is wrong, have tried many as I...

vendor by Associate II
  • 1227 Views
  • 2 replies
  • 0 kudos

Half-duplex USART ?

Posted on February 11, 2014 at 22:28 Hi, I'd like to use the USART3 of the STM32F407 (Discovery Board) in Half Duplex to control a Dynamixel AX12A. My USART initialization is the following: void USART3_init(void) { GPIO_Init...

STM32F4 - Flash stall -- more info

Posted on February 12, 2014 at 15:07I have been reading conflicting reports on writing/reading to/from FLASH when running your program code from FLASH as well.First of all, where is there documentation saying that you can stall the processor by doin...

dibs by Associate II
  • 2314 Views
  • 5 replies
  • 0 kudos

First Time User

Posted on February 04, 2014 at 05:54I am using a STM32F303 Discovery board and am not really sure where to start. I am attempting to use EWARM and ST-Link Utility together. Never having downloaded code to anything more complex than Arduino, etc., I ...

jprevard by Associate II
  • 6464 Views
  • 15 replies
  • 0 kudos

STM32F429 Discovery-Board: How to use CAN-BUS?

Posted on February 12, 2014 at 16:41Hi,I try to use one of the two CAN-BUS with the STM32F429 Discovery-Board, but seem's to be no free Port to connect the CAN-Transreceiver there.Anyone has a solution for this Problem?Regards, Michael #stm32f429...

namen by Associate
  • 1718 Views
  • 1 replies
  • 0 kudos

ST-Link STM32F103 firmware

Posted on February 03, 2014 at 16:29Hi, We are currently working on a STM32F429-EVAL board and our application works fine. We are about to make our own hardware and we want to include the same functionalities as the Eval board, including the ST-Lin...

celdran by Associate II
  • 3107 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.