2014-02-11 1:28 PM
Hi,
I'd like to use the USART3 of the STM32F407 (Discovery Board) in Half Duplex to control a Dynamixel AX12A. My USART initialization is the following:void USART3_init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* Enable GPIO clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
/* Enable UART clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* Connect PXx to USARTx_Tx*/
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3);
/* Configure USART Tx as alternate function */
GPIO_InitStructure.GPIO_OType = GPIO_Mode_IN; // Input (could also use Open Drain)
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 1000000;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_HalfDuplexCmd(USART3, ENABLE);
/* USART configuration */
USART_Init(USART3, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART3, ENABLE);
}
The TX part seems to work fine.
The problem is that the device answers (oscilloscope) but I have no RX flag when doing a simple check:
while (USART_GetFlagStatus(USART3, USART_FLAG_RXNE) == RESET);
Is my configuration correct ? How can I activate the RX part ?
And also, is there any trick to disable/enable RX on the fly ? (I can get a RX flag on my own emission but not on the answer)
Thanks!
#half-duplex-usart
2014-02-11 2:14 PM
I might initialize it thusly
void USART3_init(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* Enable GPIO clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
/* Enable UART clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* Connect PXx to USARTx_Tx*/
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_USART3);
/* Configure USART Tx as alternate function */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_Init(GPIOD, &GPIO_InitStructure);
USART_InitStructure.USART_BaudRate = 1000000;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* USART configuration */
USART_Init(USART3, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART3, ENABLE);
USART_HalfDuplexCmd(USART3, ENABLE);
}
Not sure there is any magic to half-duplex, you might want to dig up SmartCard or RS485 type examples.
You should be able to play with the RX/TX enable bits of the control register.
If you can receive your own transmissions, I'd start looking very carefully at the bit timing of the slave response, and the format/framing.
2014-02-12 12:01 PM
Thanks!
Your configuration doesn't change the result : /.The timing seems to be good since I'm doing a polling of the RX flag after my emission and I see the answer coming during this period (100µs after the emission). For the RE bit, I don't understand how I can change its status only USART3. USART_CR1 control register seems common for all USART in the Reference manual...2014-02-12 12:27 PM
USART1->CR1 != USART2->CR1
The peripherals are step-and-repeat, each has their own registers, offset from their own unique base address.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.