2014-02-13 12:34 AM
Good day,
Like topic said, the alarm handler does not to work, but if I do like this:while (!RTC_GetITStatus(RTC_IT_ALRA));printf(''\nALARM''); //it works
Here is my code: int main(void){ NVIC_InitTypeDef NVIC_InitStructure; STM_EVAL_PBInit(BUTTON_USER , BUTTON_MODE_EXTI); STM_EVAL_LEDInit(LED3); STM_EVAL_LEDInit(LED4); STM_EVAL_LEDInit(LED5); STM_EVAL_LEDInit(LED6); /* Turn LED2 ON */ STM_EVAL_LEDOn(LED3); DBGU_Init(); RTC_Config(); RTC_TimeShow(); RTC_AlarmShow(); NVIC_InitStructure.NVIC_IRQChannel = RTC_Alarm_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); while (!RTC_GetITStatus(RTC_IT_ALRA));printf(''\nALARM''); //works while(1);}and handler:void RTC_Alarm_IRQHandler(void)
{ if(RTC_GetITStatus(RTC_IT_ALRA) != RESET) { STM_EVAL_LEDToggle(LED6); RTC_ClearITPendingBit(RTC_IT_ALRA); EXTI_ClearITPendingBit(USER_BUTTON_EXTI_LINE); } }2014-02-13 1:18 AM
Hi
You have not said which STM32 Discovery board you are using. You have not shown your code for ''RTC_Config();
'' Have you done this : ''All RTC interrupts are connected to the EXTI controller. To enable the RTC Alarm interrupt, the following sequence is required: 1. Configure and enable the EXTI Line 17 in interrupt mode and select the rising edge sensitivity. 2. Configure and enable the RTC_Alarm IRQ channel in the NVIC. 3. Configure the RTC to generate RTC alarms (Alarm A or Alarm B). To enable the RTC Wakeup interrupt, the following sequence is required: 1. Configure and enable the EXTI Line 22 in interrupt mode and select the rising edge sensitivity. 2. Configure and enable the RTC_WKUP IRQ channel in the NVIC. 3. Configure the RTC to generate the RTC wakeup timer event.'' (Take from the reference manual)2014-02-13 1:30 AM
Why do I need EXTI line for that? I use STM32F4-DISCOVERY.
static void RTC_Config(void)
{ RTC_DateTypeDef RTC_DateStructure; /* Enable the PWR clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); /* Allow access to RTC */ PWR_BackupAccessCmd(ENABLE); RCC_LSEConfig(RCC_LSE_ON); /* Wait till LSE is ready */ while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) { } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE); /* ck_spre(1Hz) = RTCCLK(LSE) /(uwAsynchPrediv + 1)*(uwSynchPrediv + 1)*/ uwSynchPrediv = 0xFF; uwAsynchPrediv = 0x7F; /* Enable the RTC Clock */ RCC_RTCCLKCmd(ENABLE); /* Wait for RTC APB registers synchronisation */ RTC_WaitForSynchro(); /* Configure the RTC data register and RTC prescaler */ RTC_InitStructure.RTC_AsynchPrediv = uwAsynchPrediv; RTC_InitStructure.RTC_SynchPrediv = uwSynchPrediv; RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24; RTC_Init(&RTC_InitStructure); /* Set the alarm 05h:20min:30s */ RTC_AlarmStructure.RTC_AlarmTime.RTC_H12 = RTC_H12_AM; RTC_AlarmStructure.RTC_AlarmTime.RTC_Hours = 0x05; RTC_AlarmStructure.RTC_AlarmTime.RTC_Minutes = 0x20; RTC_AlarmStructure.RTC_AlarmTime.RTC_Seconds = 0x05; RTC_AlarmStructure.RTC_AlarmDateWeekDay = 0x31; RTC_AlarmStructure.RTC_AlarmDateWeekDaySel = RTC_AlarmDateWeekDaySel_Date; RTC_AlarmStructure.RTC_AlarmMask = RTC_AlarmMask_DateWeekDay; /* Configure the RTC Alarm A register */ RTC_SetAlarm(RTC_Format_BCD, RTC_Alarm_A, &RTC_AlarmStructure); /* Enable RTC Alarm A Interrupt */ RTC_ITConfig(RTC_IT_ALRA, ENABLE); /* Enable the alarm */ RTC_AlarmCmd(RTC_Alarm_A, ENABLE); RTC_ClearFlag(RTC_FLAG_ALRAF); /* Set the date: Friday January 11th 2013 */ RTC_DateStructure.RTC_Year = 0x13; RTC_DateStructure.RTC_Month = RTC_Month_January; RTC_DateStructure.RTC_Date = 0x11; RTC_DateStructure.RTC_WeekDay = RTC_Weekday_Saturday; RTC_SetDate(RTC_Format_BCD, &RTC_DateStructure); /* Set the time to 05h 20mn 00s AM */ RTC_TimeStructure.RTC_H12 = RTC_H12_AM; RTC_TimeStructure.RTC_Hours = 0x05; RTC_TimeStructure.RTC_Minutes = 0x20; RTC_TimeStructure.RTC_Seconds = 0x00; RTC_SetTime(RTC_Format_BCD, &RTC_TimeStructure); }2014-02-13 1:41 AM
''Why do I need EXTI line for that?''
The Reference manual says so. ''/* Enable RTC Alarm A Interrupt */
RTC_ITConfig(RTC_IT_ALRA, ENABLE);'' Check this does what the reference manual says.2014-02-13 1:46 AM
Hi
Also, just spotted you are missing this : NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4); Since your project is so simple - it does not matter which group you pick.2014-02-13 2:29 AM
Actually you were right I need EXTI, and handler worked
/* EXTI configuration */
EXTI_ClearITPendingBit(EXTI_Line17);EXTI_InitStructure.EXTI_Line = EXTI_Line17;EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;EXTI_InitStructure.EXTI_LineCmd = ENABLE;EXTI_Init(&EXTI_InitStructure);And I do not need this:NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);About alarms, can I do it on other day? I just saw that I could only set up alarm time..Thank you,//Nikolaj2014-02-13 3:08 AM
Hi
I have not used the RTC peripheral myself (yet). Looking at the RTC registers, it implies you can set any day and time. By implication : ''About alarms, can I do it on other day? I just saw that I could only set up alarm time..'' Yes - you should be able to set the alarm for another day. It CANNOT set an alarm in another month or year.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.