2014-05-08 12:28 AM
Dear ST;
I want to Optimize my program,so for the safety,I need the self-test library.but I can not find it on the st.com,so I come here to get help from you guys. Thanks very much. Yours, liuwei #stm32f10x #stm32 #certification #vde2014-05-08 1:02 AM
I want to Optimize my program,so for the safety,I need the self-test library
I'm not aware that any such thing exists for STM32. If you need safety features, I suggest to have a look at Cortex R controllers (like the TI Hercules series) which, AFAIK, implement such features in hardware.
2014-05-08 1:09 AM
I'm quite that the library exists. I found some people also look for it.but there is no answer.I hope I can get what I want.
2014-05-08 1:10 AM
2014-05-08 1:18 AM
I'm quite that the library exists. I found some people also look for it.but there is no answer.I hope I can get what I want.
Seems you are right, only that ST provides it just to ''selected'' customers. But having seem SIL3 device solutions with two identical MCUs, specialized MCU which support that features in hardware seem a better solution to me.
2014-05-08 1:46 AM
I have got one from some people long time ago,but it is too old,it's 1.2 version , now the firmware library is 3.5 version ,it has a big difference to the old version, I'm not really understand about the cpu inside things,so I can not transplant it .the question bothered me for a long time...
2014-05-08 4:12 AM
Put in a request with your local ST rep or FAE, the forum is not the place to secure limited distribution or NDA'd material.
2014-05-13 12:25 AM
2014-05-14 8:33 AM
Hi,
Sorry, the STM32F10x_StdPeriph_Lib_V3.5.0 is not certified by VDE.For more information please refer to this application note:http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/CD00290100.pdfWith regards.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.