STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Project using STM32F030K6 device

Posted on June 02, 2014 at 13:14Good day friends, Am using STM32F030K6 device for my project. I had met some issue related to SWD, BOOT0/1, Flash and USART things. So i want to know anyone who knows about this device . -welcome.

abilashs by Associate II
  • 1253 Views
  • 2 replies
  • 0 kudos

32F429I discovery power off LCD

Posted on May 30, 2014 at 14:14Hi,I have a 32F429I discovery board and I am trying to put it into sleep mode using a call to HAL_PWR_EnterSTOPMode . I believe that this works, but I would also like to turn off the display when doing this.Is there an...

mats23 by Associate II
  • 798 Views
  • 2 replies
  • 0 kudos

STM32F3 USB

Posted on February 10, 2014 at 17:48Hello,I've downloaded the custom-hid program on the STM32F3 Discovery . I've alsoinstalled the usb hid demonstrator. But it doesn't recognise any 'USBHID target'. How can I make the host talkto my board? Will it h...

hilwan by Associate II
  • 3143 Views
  • 11 replies
  • 0 kudos

STM32F4 Discovery, cannot clear parity error intterrupt

Posted on June 02, 2014 at 04:16Hello, I'm using STM32F4 discovery to develop usart communication function. The usart parameter is below. /// Set serial port  USART_StructInit(&USART_InitStructure);  USART_InitStructure.USART_BaudRate = 9600;      ...

takeda by Associate
  • 1647 Views
  • 3 replies
  • 0 kudos

DMA configuration for FSMC

Posted on May 31, 2014 at 12:45Hey, I am presently transferring an image from a camera (connected through DCMI) to the internal SRAM via the DMA. This way I'm able to get the whole image. However, when I try to write into the external SRAM through t...

kai2 by Associate
  • 1592 Views
  • 2 replies
  • 0 kudos

STM32F4 - MPU-6050 cannot communicate ...

Posted on May 31, 2014 at 21:37Hello Friends, I bought stm32f4 discv. board and also http://www.aliexpress.com/item/1-pcs-MPU-6050-Module-3-Axis-Gyroscope-Accelerometer-Module-for-Arduino-MPU-6050-Worldwide-FreeShipping/1361575363.html board but i h...

aybala5 by Associate II
  • 2172 Views
  • 3 replies
  • 0 kudos

STM3221G-EVAL LCD STAYS AT WHITE

Posted on May 31, 2014 at 16:56Hi everyone, I have just opened my STM3221G-Eval and created the default program for it using IAR Workbench for ARM 7.10. I first wanted to know whether why my  LCD stays at white. Thanks

STM32F105RB problem

Posted on May 30, 2014 at 15:57 Hi, I am facing a problem with the MCU model STM32F105RB. I am using it with the J-link EDU. I use a custom hardware, which works properly with the STM32F205RB model. Now I am trying to use the same c...

Disable JTAG-DP + SW-DP for STM32F303

Posted on May 28, 2014 at 08:40 Hi, I have been looking around in the forums for a solution for my target mcu, STM32F I want to use the I2C1_SDA/SCL on PA14/PA These pins are used for JTA-DP and SW-DP. I want to disable this and use only the I2C...

vaibhav23 by Associate II
  • 3459 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.