2014-05-30 2:09 AM
I compiled the micro STM32F05k4U6 using the IAR Embedded Workbench for ARM 6.40.2 and I get a binary
When I tried to program the binary using the STM32 ST-Link Utility the binary gets download but when I power up the board the binary is not really loaded. I think must be some property in the IAR Embedded Workbench that must not be well configured. Best regards, Estanis2014-05-30 2:17 AM
Hi
Yes, this one use to catch me out all the time. In IAR, they provide a simulator, it is the default target! Make sure under targets, you select the ST-link as the target debugger (not the simulator).2014-05-30 2:21 AM
Thanks for the response.
Do you have some example of IAR embededd project properties I can see? Best regards,2014-05-30 2:49 AM
Hi
''Do you have some example of IAR embededd project properties I can see?'' Unfortunately not at the moment, the company I work at now uses Atollic (I do not recommend it!). I believe there are many IAR projects in the standard peripheral Library http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF2578842014-05-31 7:04 AM
Hi
OK, so I have my laptopn now and have grabbed this screen shot for you. Select the debuger option in left pane. In the debugger tab (right pane) - in the 'Driver' drop down list - select the ST-Link (instead of simulator) ________________ Attachments : IAR_Settings.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I18m&d=%2Fa%2F0X0000000biw%2F0hK90AK3HasFgHo0lgxMJzd5zALDqcl_N65uKWekR7U&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.