STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART Send String Problem

Posted on May 30, 2014 at 09:57Hi, I need your help...I try to use the USART1 of the STM32F107 to send a string (''HELLO WORLD'') but on the hyperterminal, I receive just the first letter (''H''). I cannot found the fault, I use Coocox CoIDE with th...

damncm by Associate
  • 1847 Views
  • 3 replies
  • 0 kudos

Interrupt Nesting on STM32F3Discovery

Posted on May 30, 2014 at 15:15 Hi Is there a way to disable interrupt nesting (preemption) on the STM32F3Discovery? By default, an interrupt seems to preempt a currently executing ISR. But I want the ISRs (especially those of DMA and EXT...

STM32F051 Comparator inverting input

Posted on May 05, 2014 at 08:19Hello I use the comparator module of a STM32F051. The problem is that I need to change the input pin of the inverting input on the fly. In the datasheet, for COMP1 module, the input pins PA0, PA4 and PA5 are possible s...

DAC output changes ADC reading

Posted on May 21, 2014 at 00:25Hi,I'm using the STM32F4 Discovery board. I have a program that outputs voltages with the onboard DAC and reads voltages with the ADC. For some reason when the DAC is outputs a voltage it lowers the readings of the ADC...

bridges by Associate II
  • 3510 Views
  • 8 replies
  • 0 kudos

Question on STM32 DMA FIFO

Posted on February 14, 2014 at 18:01Hi All,reading the reference manual of the STM32, I have a question related to a transfer peripheral to memory using DMA, direct mode ( no FIFO )In section 9.3.12, Direct Mode paragraph, i found:Direct modeBy defa...

STM32F427ZI USB

Posted on May 28, 2014 at 20:27Hello again Gentlemen!I would like to download some sample code to help me to program the USB peripheral to use it as a Virtual COM port. I guess on the PC side I have to install the ST Micro Virtual COM port driver, r...

gmotta by Associate II
  • 2022 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.