STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX bugs

Posted on April 06, 2014 at 14:25Hi all,I just started developing with the STM32F4 Discovery board and I've been trying to use STM32CubeMX for code generation.Until now, almost every configuration I tested didn't work, that means STM32CubeMX (I'll c...

shippo by Associate II
  • 2968 Views
  • 7 replies
  • 0 kudos

array to string in usart peripheral

Posted on June 06, 2014 at 16:02i know about usart, for transmited by transmittter and received data by receiver i can do it.. i communication usart use looping and use array too... how can i make this array to become string  so i can use function l...

gusonela by Associate II
  • 3050 Views
  • 7 replies
  • 0 kudos

Timer Input Capture on Both Rising and Falling Edge

Posted on June 06, 2014 at 13:14Hi all,           Presently i am capturing input signal only on its rising edge and also i can capture the same signal only on its falling edge. But i need to capture on both rising and falling edges, please let me kn...

A stupid question about GPIO input mode

Posted on June 07, 2014 at 00:56Hi ST,I'm using ST32F4Discovery board, and I want to read a 4 bit data that is continuously streaming in. I'm thinking of doing:1. set GPIO port for the input (say PA10)2. call this function to read data: GPIO_ReadInp...

Problem trying to write a timer program counting edges

Posted on June 06, 2014 at 02:06Hey ST,I'm using STM32F4DISCOVERY board, and tried to write a counter for rising and falling edges using timer input capture mode. Couldn't capture anything though. Any ideas what's wrong would be appreciated.Also, do...

STM32F0308DISCOVERY Bootloader Go-Command

Posted on June 06, 2014 at 11:00HiThe bootloader GO command doesn�t work as expected. Generally AN3155 is wrong here, because the second ACK after the address isn�t send also on other chips (STM32F2, STM32F4, �), but the jump works there.Test system...

franz2399 by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos

STM32F4: UART not transmitting

Posted on June 05, 2014 at 16:16Hi,I am currently working on an application that will send/receive time and date data through serial connection via UART. To get a prototype up and running, I modified the RTC calendar example code that comes with STM...

tyx3gu by Associate II
  • 3276 Views
  • 6 replies
  • 0 kudos

Time Base for Timer in Encoder Mode

Posted on June 06, 2014 at 05:13 Hi , I came across the following codes . TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Period = 0xffff; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure....

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.