2014-06-06 2:00 AM
Hi
The bootloader GO command doesn�t work as expected. Generally AN3155 is wrong here, because the second ACK after the address isn�t send also on other chips (STM32F2, STM32F4, �), but the jump works there.
Test system:
Hardware
:
STM32F0308DISCOVERYhttp://www.st.com/web/en/catalog/tools/PF259100
Firmware
http://www.st.com/web/en/catalog/tools/PF259447
-> STSW-STM32140
programmed with
JTAG
Serial tracing after reset (bootloader mode enabled)
No
Packet
Start Bit
Data bytes
Parity Bit
Stop Bit
Error
Start Time
End Time
1
Data
0
7F
1
1
-
101,9ms
102ms
Enter bootloader
1
Data
0
79
1
1
-
102ms
102,1ms
2
Data
0
21
0
1
-
134,3ms
134,4ms
Start Go
3
Data
0
DE
0
1
-
134,4ms
134,5ms
2
Data
0
79
1
1
-
134,5ms
134,6ms
4
Data
0
08
1
1
-
154,2ms
154,3ms
Send Address
5
Data
0
00
0
1
-
154,3ms
154,4ms
6
Data
0
00
0
1
-
154,4ms
154,5ms
7
Data
0
00
0
1
-
154,5ms
154,6ms
8
Data
0
08
1
1
-
154,6ms
154,7ms
3
Data
0
79
1
1
-
154,7ms
154,8ms
Confirm receiving address and checksum
Missing confirmation for valid address and checksum
After that sequence, the MCU stays in bootloader!
referenced
m
anuals
AN2606 Application note STM32� microcontroller system memory boot mode Rev 5 AN3155 Application note USART protocol used in the STM32� bootloader Rev 17Additional information
WR 7F
RD 79 WR 00 FF RD 79 RD 0B RD 31 RD 00 01 02 11 21 31 44 63 73 82 92 RD 79Version: 3.1
Supported Commands: ExtendedEraseMemory True EraseMemory False ReadMemory True ReadoutProdect True Go True ReadoutUnprodect True WriteProdect True WriteUnprodect True WriteMemory True GetID True GetVersionAndReadProtectionStatus True GetVersionAndAllowedCommands TrueAny ideas would be most welcome.
Thanks #stm32f030-bootloader-go2014-06-06 8:31 AM
I guess I'd start by looking closely at what code I was executing, and if there is a watchdog you need to keep kicking. Technically the code could return to the System Loader, it could watchdog, or hard fault. Code called in flash is probably not mapped at zero, but I'd need to do more analysis.
From another F0 ROM1FFFF334 LOC loc_1FFFF334_GoCmd: ; Xref 1FFFF294
1FFFF334 F7FF FF5D bl sub_1FFFF1F2_GetUsartDWORD
1FFFF338 4604 mov r4, r0
1FFFF33A F7FF FDD1 bl CheckMemRegion
1FFFF33E B2C0 uxtb r0, r0
1FFFF340 2802 cmp r0, #2
1FFFF342 D001 beq.n loc_1FFFF348
1FFFF344 2803 cmp r0, #3
1FFFF346 D10A bne.n loc_1FFFF35E_SendNACK
1FFFF348 LOC loc_1FFFF348: ; Xref 1FFFF342
1FFFF348 F7FF FD96 bl sub_1FFFEE78
1FFFF34C F7FF FCB9 bl sub_1FFFECC2_EnableInt
1FFFF350 6865 ldr r5, [r4, #4] ; +4 PC
1FFFF352 6820 ldr r0, [r4, #0] ; +0 SP
1FFFF354 F7FF FCB0 bl sub_1FFFECB8_SetMainStack
1FFFF358 47A8 blx r5 ; GO
1FFFF35A E77F b.n loc_1FFFF25C_CmdLoop
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.