2014-06-06 3:56 PM
Hi ST,
I'm using ST32F4Discovery board, and I want to read a 4 bit data that is continuously streaming in. I'm thinking of doing:1. set GPIO port for the input (say PA10)2. call this function to read data: GPIO_ReadInputDataBit(GPIOA, GPIO_PIN_10)Would this work?Also, i just wanted to ask how can you even use the function GPIO_ReadInputData (in the GPIO library) if it has no pin# as input parameter?uint8_t GPIO_ReadInputDataBit(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin);uint16_t GPIO_ReadInputData(GPIO_TypeDef* GPIOx);Also, is there a way to do this in DMA mode? read input 4-bit data and go straight into memory.2014-06-06 4:22 PM
GPIOx->IDR reads all 16 pins in the bank as a 16-bit variable, you can shift and mask multiple pins from that.
Say 4-bits at PC10,11,12,13 data = (GPIOC->IDR >> 10) & 0x0F; Yes, you can use DMA, and have DMA clocked via a TIM, or an external clock routed through a TIM. You can DMA in or out. I've posted several examples, and it has been discussed in a couple of threads. You can just to 4-bit, you basically get to read 16-bit and then post process the data to extract those of interest to you. For DMA out, basically I think 8-bit or 16-bit at byte/word boundaries is viable. Say you wanted to pump PCM audio data to a resistor chain/ladder DACWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.