STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Change heap size in IAR embedded workbench

Posted on July 29, 2014 at 21:07HiI'm trying to get the USB virual com ports working with a STM32F401 discovery board, using IAR workbench, and the code generated from STM32 Cube MX. I found this/public/STe2ecommunities/mcu/Lists/STM32Java/flat.aspx...

bgeri91 by Associate
  • 2315 Views
  • 2 replies
  • 0 kudos

Reading Problem from ADC

Posted on July 29, 2014 at 00:53Hello,        I am reading from an external ADC in parallel interface(16 bits). I dont know what is wrong, only my port PE0 and PE1 are talking to the controller at 1V and rest all others taking at 3V. when I remove t...

DFU mode driver v3.0.4

Posted on February 03, 2014 at 17:30The DFUse software package (STSW-STM32080, version 3.0.3) comes with the USB Tube driver (STTub30.sys) version 3.0.1.  This driver works for me on Windows 7, but does not work on Windows 8 for me.  At some point i...

32L0538DISCOVERY

Posted on July 28, 2014 at 11:51Hi everyone,I apologize beforehand if this isn't the right place to post my question, but I just started with this forum :).Anyway, I've been given an STM32L0538-Discovery board for a project and I can't seem to find ...

zehpaulo by Associate
  • 1237 Views
  • 3 replies
  • 0 kudos

WFI() debugging

Posted on July 25, 2014 at 18:47I have used WFI() previously, but I can't figure out what is going on with my current code.  The WFI() returns immediately, but I can't figure out what interrupt is active.  Any tips for determining what caused a WFI(...

mreuter by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

HID Packet Taking Too Long at FS USB

Posted on July 28, 2014 at 01:25I have two different projects: one based on the '205, one on the '427, Both use identical USB libraries from ST. They are both set up as FS devices using the internal USB PHY. The issue I am seeing is that in the '205...

jvavra by Associate III
  • 1386 Views
  • 3 replies
  • 0 kudos

Reduce Amplitude obviously

Posted on July 27, 2014 at 15:28When I using my desktop computer to power the STM32F429i Disco, the PWM out put amplitude is aobut 3v, but when I use a IC LM7805 (change DC form 9V to 5V) to power it, PWM reduce amplitude obviously, even just have 1...

Linda by Associate II
  • 1521 Views
  • 3 replies
  • 0 kudos

ADC_DR Register always empty

Posted on July 28, 2014 at 11:40 Hi All, I'm trying to use the ADC1 GPIO G8 from the STM32F207IG. Unfortunately I don't get it working and maybe someone could help me. The basic problem is that all ADC_*** registers getting updated e...

b_ by Associate II
  • 2211 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.