2014-07-27 6:28 AM
When I using my desktop computer to power the STM32F429i Disco, the PWM out put amplitude is aobut 3v, but when I use a IC LM7805 (change DC form 9V to 5V) to power it, PWM reduce amplitude obviously, even just have 1%.
Please help. Thanks2014-07-27 4:52 PM
So 0.03V?
Assume no one here knows how you've wired this up, or the voltages at key test points.2014-07-28 8:43 AM
I have not wired it up with anything yet. Even I wired up with some circuit, the same result.
When I use USB from my desktop computer, the P1(5V) is 4.58, when use LM7805, it is 4.55. not much different. But when test point I should look into? Thnaks2014-07-28 9:10 AM
As you're complaining about output voltages from the processor, perhaps start there, and verify the supplies, and outputs of VCAP pins. The voltages across the capacitors might be the easiest to scope.
Where exactly are you injecting your 5V supply? I'd perhaps use the USB USER port, or via diode to the 5V pin on P1We’re moving the ST Community to a new platform to give you a better and more reliable community experience.