2014-08-21 9:05 PM
Hello,
I load several example projects unmodified into Keil and compile as soon as I enter. When the project enters the linking phase, I get an error that HAL_DMA_Init is an undefined symbol, and the project won't compile. Is there any reason for this? This happens with UART, I2C, and SPI examples right out of the box before I have a chance to modify. This is on the STM429I-Discovery\Examples software. The specific issue is ''not enough information to list image symbols''. Thanks David Bassett2014-08-22 4:07 AM
I load several example projects unmodified into Keil and compile as soon as I enter. When the project enters the linking phase, I get an error that HAL_DMA_Init is an undefined symbol, and the project won't compile.
Perhaps another version of uVision, and less-than-perfect project import. Adding the corresponding source file to the project should correct this issue. However, I wouldn't be surprised if more such trouble follows.
2014-08-22 7:06 PM
Hello,
I have an update here which solved the problem. It appears the issue tracked everything which had DMA in it, and when I diffed my version of stm32f4xx_hal_dma.c with the original, The WHOLE function definition in the Keil project was gone from the function definition to the end brace. I figure the odds of inadvertently highlighting and deleting a function right from the definition to the ending brace are like one in a billion, I assume Keil version 5.10 had something to do with this, but I don't know how. When I replaced the function back into hal_dma.c, things worked fine again. Dave BassettWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.