STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f4 SPI spurious Interrupt problem

Posted on August 27, 2014 at 09:47Hello,Kindly help me resolve the STM32F4 SPI interrupt problem.I am trying to connect two stm32f4 boards, one of it is stm32f439 evaluation board and other one is stm32f407 based my development board. I am testing i...

jagdish by Associate II
  • 1182 Views
  • 1 replies
  • 0 kudos

Where can I find the UM1725 user manual?

Posted on April 15, 2014 at 11:28Hi all, it is stated within the UM1718 user manual that ''the following documents are available from http://www.st.com:''; Description of STM32F4xx HAL driver user manual (UM1725) and Description of STM32F2xx HAL dr...

jamsoft by Associate II
  • 5746 Views
  • 9 replies
  • 0 kudos

Problems due to STM32F417 Silicone Revision 1?

Posted on August 26, 2014 at 16:44Dear community, one of our products uses a STM32F417IGH6 controller and has previously been build using silicone revisions A and Z. The current batch is the first with silicone revision 1 and serveral problems came...

bve by Associate II
  • 2135 Views
  • 4 replies
  • 0 kudos

STM32Cube_FW_F2_V1.1.0 Documentation location ?

Posted on August 22, 2014 at 11:43I have downloaded the STM32Cube_FW_F2_V1.1.0 package and trying to use the STM32F2xx_HAL_Driver with a STM32F205RET6. Where to find the latest HAL documentation? (The ''Documentation'' folder in the zip was empty)

bjorn23 by Associate
  • 1245 Views
  • 2 replies
  • 0 kudos

STM32F030F4

Posted on August 25, 2014 at 21:10Please where can I find correct header files for the 20 pin STM32F030F4 devices? Cheers Felix

felix2 by Associate II
  • 1660 Views
  • 3 replies
  • 0 kudos

[STM32f4-Discovery] I2S RX Master with DMA

Posted on March 06, 2013 at 19:44 Hi I have some questions for the following scenario. I want to configure the dma controller to transfer data from an digital i2s mems microphone to the memory. The I2S (SPI2) is the rx master and the memor...

Set USART2_RTS when GPIO is in alternate function mode.

Posted on August 25, 2014 at 16:06I have a STM32L152RCT6 mcu and a bluetooth module connected to usart2. I've also set up the dma for the communication. The gpio is set to alternate function mode. It works, however sometimes a packet loss happens. T...

zoltan by Associate
  • 1204 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.