STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Input Capture issue

Posted on August 28, 2014 at 01:04Hi:I am using the STM3221G-EVAL board and TIM example from STM32F2xx_StdPeriph_Lib. I modified the original example so I can use PG15 input.There is a pushbutton connected to PG15 on the eval board.When I press the ...

eduardo2 by Associate II
  • 1520 Views
  • 2 replies
  • 0 kudos

STM32CubeMX / HAL Bug Report: PLLSAI

Posted on July 14, 2014 at 02:29 In trying to compile generated code from the STM32CubeMX application for the STM32F429I-DISCO board, I've found a problem with part of the HAL library. Simply, the PLLSAI assert #defines have a bug in thei...

evan23 by Associate II
  • 1401 Views
  • 2 replies
  • 0 kudos

VCP on Nucleo : What's wrong ?

Posted on August 25, 2014 at 16:33Hello, I'm developping an internal production tool that uses a nucleo as MCU board. It uses the built in VCP to communicate with a .NET application. I'm using vitual com ports on many many apps and never had such pr...

root by Associate II
  • 1738 Views
  • 2 replies
  • 0 kudos

SDIO TX underrun because of DMA FIFO error

Posted on October 05, 2012 at 15:03Hello,we are trying to work with SDIO at our FreeRTOS project, Without FreeRTOS everything works fine @ 16 MHz with Transcend miscroSDHC card, but if we try to do same test as FreeRTOS thread, we get TX underrun co...

rerayne by Associate II
  • 3261 Views
  • 6 replies
  • 0 kudos

Configuring uClinux for STM32

Posted on August 25, 2014 at 15:32Hi. I am configuring uClinux for STM32F1. I have applied the STM32 patch. But, in the uClinux-dist/vendors, I am unable to find the STM32 folder. Besides, after menu makeconfig, I cannot find the vendor selection ta...

shauns87 by Associate II
  • 2377 Views
  • 4 replies
  • 0 kudos

STM32L152 Flash Access

Posted on August 27, 2014 at 17:19 Hello Everyone, I am working on an STM32L152 based platform and trying place some data inside internal flash. As you may know, when a page is erased, in stm32L1, each bit is set to 0x00 instead of 0xFF....

emeydanli by Associate II
  • 1760 Views
  • 3 replies
  • 0 kudos

Unable to use USART1_TX PA9 pin because of USB conflict?

Posted on August 22, 2014 at 17:09 Hello everybody! It's not my first experience with USART but this time I have an unsolvable problem :) I try to use USART1 TX with the pin PA9 but I can't send datas. The pin PA9 always outputs 1.1V and...

jean by Senior
  • 3663 Views
  • 8 replies
  • 0 kudos

stm32f100 U(S)ART and busy flag

Posted on August 25, 2014 at 19:58I read the reference manual for circuit mentioned but I cannot find any flag in register for USART that will show there is some transmission/reception active. Is there someone who solved similar problem? I need this...

semler by Associate II
  • 2572 Views
  • 6 replies
  • 0 kudos

Getting absolute variable addresses for STM studio

Posted on August 27, 2014 at 13:08HiI am using the stm32f072b discovery board for a project I am doing at my university.  I want to read values from the gyroscope and read them using stm studio. How would I found out where the address for the absolu...

16270827 by Associate
  • 1171 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.