2014-08-27 4:04 PM
Hi:
I am using the STM3221G-EVAL board and TIM example from STM32F2xx_StdPeriph_Lib. I modified the original example so I can use PG15 input.There is a pushbutton connected to PG15 on the eval board.When I press the pushbutton nothing happens. The system never goes through TIM1_CC_IRQHandler. what would be the problem?Thanks.int main(void){ /*!< At this stage the microcontroller clock setting is already configured, this is done through SystemInit() function which is called from startup file (startup_stm32f2xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f2xx.c file */ /* TIM1 Configuration */ GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; TIM_ICInitTypeDef TIM_ICInitStructure; /* TIM1 clock enable */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); /* GPIOG clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); /* TIM1 channel 2 pin (PG.15) configuration */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOG, &GPIO_InitStructure); /* Connect TIM pins to AF1 */ GPIO_PinAFConfig(GPIOG, GPIO_PinSource15, GPIO_AF_TIM1); /* Enable the TIM1 global Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM1_CC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* TIM1 configuration: Input Capture mode --------------------- The external signal is connected to TIM1 CH2 pin (PG.15) The Rising edge is used as active edge, The TIM1 CCR2 is used to compute the frequency value ------------------------------------------------------------ */ TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV8; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM1, &TIM_ICInitStructure); /* TIM enable counter */ TIM_Cmd(TIM1, ENABLE); /* Enable the CC2 Interrupt Request */ TIM_ITConfig(TIM1, TIM_IT_CC2, ENABLE); while (1);}void TIM1_CC_IRQHandler(void){ if(TIM_GetITStatus(TIM1, TIM_IT_CC2) == SET) { /* Clear TIM1 Capture compare interrupt pending bit */ TIM_ClearITPendingBit(TIM1, TIM_IT_CC2); if(CaptureNumber == 0) { /* Get the Input Capture value */ IC3ReadValue1 = TIM_GetCapture2(TIM1); CaptureNumber = 1; } else if(CaptureNumber == 1) { /* Get the Input Capture value */ IC3ReadValue2 = TIM_GetCapture2(TIM1); /* Capture computation */ if (IC3ReadValue2 > IC3ReadValue1) { Capture = (IC3ReadValue2 - IC3ReadValue1); } else if (IC3ReadValue2 < IC3ReadValue1) { Capture = ((0xFFFF - IC3ReadValue1) + IC3ReadValue2); } else { Capture = 0; } /* Frequency computation */ TIM1Freq = (uint32_t) SystemCoreClock / Capture; CaptureNumber = 0; } }} #input-capture #stm3221-eval2014-08-27 7:24 PM
I am using the STM3221G-EVAL board and TIM example from STM32F2xx_StdPeriph_Lib. I modified the original example so I can use PG15 input.There is a pushbutton connected to PG15 on the eval board. When I press the pushbutton nothing happens. The system never goes through TIM1_CC_IRQHandler. what would be the problem?
Problem is that PG15 has no association with TIM1, you might want to review the part's Data Sheet.2014-08-28 5:29 AM
ok, thanks clive1.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.