STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Free IDE and Compiler for STM32Cube

Posted on August 29, 2014 at 07:13We have been looking at starting developing STM32 related products for a while now. Up till not, always concentrated on Microchip PIC. Can anyone tell me if it is possible compiling STM32Cube projects with free tool...

Code sample for AN3109 - anyone know where to find it

Posted on September 01, 2014 at 07:31I have found a couple threads here that have old (not working) links for the SW to accompany AN3109, but no luck finding the code. Anyone either have a copy of the code or know where it is hiding at ST.com?Thanks

william by Associate
  • 1191 Views
  • 1 replies
  • 0 kudos

Virtual COM Android

Posted on September 01, 2014 at 09:50Hi,We are building an Android application which communicates with the STM32 Virtual COM port. To the moment we can't get it working. Are there any Java libraries which can help us or any kind of Android applicati...

pesho1 by Associate
  • 758 Views
  • 0 replies
  • 0 kudos

Does the STM32F030 series have single-cycle multiplication?

Posted on August 31, 2014 at 15:33I am not sure if the MCU STM32F030 has single-cycle multiplication,which is based on the ARM Cortex-M0 core? Anybody knows that please help me.I want to use this MCU for motor control,is that suitable?Thanks.Best Wi...

wqluck by Associate
  • 1630 Views
  • 2 replies
  • 0 kudos

Power Source Solar Powered (stm32l152 discovery)

Posted on August 31, 2014 at 18:51I make the charger from the solar panels with automatic orientation to the sun. There is a problem after device reset, reset to zero RTC. What can cause, reset clocks?http://youtu.be/CaiQAkqU08w?list=UUrYD2NXH5n3BeO...

asv-lab by Associate
  • 1442 Views
  • 2 replies
  • 0 kudos

Nucleo STM32F401

Posted on August 30, 2014 at 22:25Problem with oscillator source PLL.Nucleo plate does't have HSE oscillator, and use internal 16 MHz HSII want to reconfigure tacting schematic to use as SYSCLK - PLL (by default for SYSCLK use HSI directly)PLL confi...

dizarker by Associate II
  • 2806 Views
  • 5 replies
  • 0 kudos

Adding an uninitialized data section to a GCC build?

Posted on December 22, 2011 at 07:18 Perhaps the subject line is a bit cryptic, but does anybody know how to add uninitialized data sections to the linker script? The F4xx has two RAM banks. I want to use the smaller 64 kB as the normal RAM area...

RTOS, adding message bus feature

Posted on August 30, 2014 at 06:42 I have an idea for freeRTOS in stm32cube and other RTOS, adding message bus feature to them! Like a CAN bus this bus operate but between tasks instead of devices. Many times a task have a message that can publish a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.