STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question about external RAM and SD

Posted on October 02, 2014 at 17:05Hello,I try to test my application with a new setup with external SRAM on the STM3240G kit, for heap and stack.I use FatFS on SDIO which needs DMA. When I read a file there is a problem.I know it is not possible to...

pcu by Associate II
  • 1992 Views
  • 3 replies
  • 0 kudos

clock division

Posted on October 02, 2014 at 21:51Hello,       I am having hard time to figure this out. in the data sheet it is mentioned that the STM32F407 works at a maximum clock of 168 Mhz, but using any module timer, PWM or any other the clock is divided by ...

Generated CubeMX code with customer API

Posted on October 01, 2014 at 09:43Hi, I'm working on stm32f4 mcu and I'm using CubeMX to generate the code useful for my applications, so I'm wondering if it is possible to generate CubeMX code using my personal API; in other words, I'd like to lin...

DUrbano by Associate III
  • 1300 Views
  • 3 replies
  • 0 kudos

STM32F302: Unable to set Register CR: ADSTART

Posted on September 30, 2014 at 23:20 I am trying to get the ADC working on a STM32F302 processor and I am noticing while single stepping the code is when I call�? HAL_StatusTypeDef HAL_ADC_Start(ADC_HandleTypeDef* hadc)�? and exercise the code t...

ebommer by Associate II
  • 3408 Views
  • 10 replies
  • 0 kudos

Pinout Spreadsheet for the STM32F4-Discovery Available

Posted on January 05, 2012 at 18:47I have created an Excel spreadsheet to help in the Discovery-F4 pin assignment process, and as a useful reference for the pin functions.  The STM32-Discovery-F4 pinout spreadsheet lists the Discovery modules pin i...

kornak by Associate II
  • 3658 Views
  • 3 replies
  • 0 kudos

Single 0V GPIO Pulse Synched w/ Timer

Posted on October 01, 2014 at 20:31Using a STM32F427, I've got TIM5 generating an 8MHz PWM output. I've also got a GPIO output that is hooked to an active LOW enable on a device that needs to be turned on every once in awhile. What I'd like to do is...

jvavra by Associate III
  • 1039 Views
  • 4 replies
  • 0 kudos

Stm32f103, hardfault problem

Posted on October 02, 2014 at 14:23Hello everyone,I've this hardfault problem for a quite long time now, I solved the issue by putting a software reset in the hardfault loop but now is not acceptable anymore.I suspect it has something to do with sen...

gnu by Associate II
  • 3280 Views
  • 2 replies
  • 0 kudos

STM32F429 discovery board USB application developpment

Posted on October 01, 2014 at 13:19Hello,I'm trying to develop a USB driver device using STM32F429 discovery board. I couldn't find any working examples that allow me to connect my board to a computer and to be detected. I would like to be detected ...

ignasi by Associate II
  • 1708 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.