STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

enable CAN1_RX0_IRQn and CAN1_SCE_IRQn

Posted on October 17, 2014 at 11:21 I have a CAN bus project that needs to use bothCAN1_RX0_IRQn and CAN1_SCE_IRQn. But it happened is that when I enabledboth of the interrupts, then the interrupts did not work at all. Here is my CanConfig(): ...

stm32f407 sram boot in linux

Posted on October 19, 2014 at 22:01Hi, I have loaded and run apps in sram using keil environment. I am working my way into linux, but i am not able to use the same feature, i have tried to load an .elf file using st-utils, openocd. but so far there ...

STM 32F4 Timers Step By Step

Posted on October 17, 2014 at 18:40 Dear All I would like to start a discuss about STM32F4 series timers operation while learning and understanding. Please share your idea and experience to explain each red circles from number 1 in the attach...

0690X0000060MmkQAE.gif
pic_micro by Associate II
  • 2459 Views
  • 4 replies
  • 0 kudos

STM32F401RE IAP

Posted on October 18, 2014 at 00:32Hi.I'm developing an application where I have to use IAP.I downloaded IAP example from this site and for F407VG it worked just great.But then problems occured.I need this on STM32F401RE. IAP file is uploaded to stm...

tm3341 by Associate II
  • 1427 Views
  • 6 replies
  • 0 kudos

TCS3200 color sensor with stm32f4

Posted on October 18, 2014 at 14:03Hi I'm trying to use TCS3200 color sensor interface with stm32f4I used input capture of timer 2, channel 3 and Interrupt to calculator pulse from OUT sensorOf course, i don't  know algorithm good. Because the senso...

41001051 by Associate II
  • 2490 Views
  • 1 replies
  • 0 kudos

STM32F429VG support 24-bit LCD TFT?

Posted on October 18, 2014 at 10:25Does STM32F429VG support 24-bit LCD TFT? It's 100 PIN LQFP and not has LCD_B1, LCD_R0, LCD_R1 pins definition in datasheet. So is it only support RGB565, and not support RGB888? Can you give me help?Thanks a lot.

ray by Associate II
  • 1506 Views
  • 3 replies
  • 0 kudos

FFT Programming(STM32f4xx)

Posted on October 18, 2014 at 08:04hi,Please someone post a sample example of fft program for stm32f4xx using cfft functions.  #learn-using-search-engines

STM32F4 what is the best I2C Comunication Method?

Posted on October 18, 2014 at 09:13Hello guys, a few months ago i started to work with discoveryF4 board and some sensors in i2c mode. But my inconvenient was that after several minutes or several hours the code just STONED... So in the last couple...

Bogdan by Senior
  • 840 Views
  • 1 replies
  • 0 kudos

ST-Link Connection error�

Posted on November 07, 2012 at 15:20I'm a student of University of Catania and I'm using IAR Embedded Workbench for ARM, v. 6.21, 32K Kickstart Edition on WIndows 7, for an university project to program a STM32F100XB board (using SWD Interface)It wo...

amedm by Associate II
  • 4183 Views
  • 10 replies
  • 0 kudos

externally triggered output compare

Posted on October 17, 2014 at 23:56I am using an STM32F4 discovery board.  I want to use an external trigger to generate an interrupt that will cause a pulse stream.  I have found examples using an external trigger for one pulse mode as well as outp...

garth by Associate
  • 823 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.