STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Decrease priority during runtime of interrupt

Posted on October 20, 2014 at 13:06Hi, I have an application where interrupts come very fast on a timer (about 100kHz). Most time this interrupt is handled very immediate, and then all is fine. This interrupt should have quite high pre-emptive prior...

flyer31 by Senior
  • 1749 Views
  • 3 replies
  • 0 kudos

Stm32L0 Nucleo - EXTI 0_1 issue

Posted on October 16, 2014 at 15:25Hi All,I'm trying to work with the STM32L0 Nucleo board and I found a strange behavior:If I configure an EXTI interrupt on line 0-1 (no matter which pin but I tryed pins PA-B-C/0-1) the interrupt is triggered immed...

STM32CubeF0 bugreport (HAL, USB, VCP)

Posted on August 06, 2014 at 09:00 Bug 1: STM32Cube_FW_F0_V1.0.0\Drivers\STM32F0xx_HAL_Driver\Inc\stm32f0xx_hal_pcd.h typedef struct { PCD_TypeDef *Instance; /*!< Register base address */ PCD_InitTypeDef Init; /*!< PCD required p...

Vddio2 usage questions

Posted on October 15, 2014 at 10:16Hello, i've an application where an STM32F072 is connected to a GSM engine which provides an I/O voltage when turned on and expects no current flow over the I/O lines into the engine when off. Using Vddio2 for this...

rg by Associate II
  • 2866 Views
  • 4 replies
  • 0 kudos

MTBF STM32F103

Posted on October 20, 2014 at 14:10I'm looking for information regarding the MTBF of the STM32F103 BGA IC. It would be helpful if someone can send me the failure rate of this microcontroller. Thanks Regards Henri #failure-rate #mtbf

henri2 by Associate
  • 942 Views
  • 0 replies
  • 0 kudos

Can I replace CMSIS ver4.20 on older versions of CMSIS files in standard peripheral library for stm32F10x and stm32F4x?

Posted on October 18, 2014 at 08:06Can I replace CMSIS ver4.20 files on older versions of CMSIS files in standard peripheral library for stm32F10x(ver3.5 or 3.6) and stm32F4x(ver1.4)? Is there any bug in this change? Is there any relation between SP...

STM32Cube Libraries PWM

Posted on October 19, 2014 at 13:38 Hi, I am trying to output two PWM signals through channels 1 & 3 of TIM3. I'm using the Nucleo F401RE board, so my MCU is STM32F401RE. I checked the example code included with the HAL and also the code generat...

SDRAM ON STM32F439I-EVAL2

Posted on October 15, 2014 at 14:54Hi I try find datasheet SDRAM on this board but I can't find it. I want Row Address Input and Column Address Input . please help me. #lmgtfy

stdavod by Associate II
  • 4070 Views
  • 14 replies
  • 0 kudos

STM32cube mx

Posted on October 13, 2014 at 14:58I have installed STM32cubeMX and have some functionality. When I do a configuration and then try to generate code the cube window locks up. I left things for 40 minutes but no change.  A project file (.ioc ) is gen...

bob23 by Associate II
  • 2771 Views
  • 6 replies
  • 0 kudos

RTC Wakeup doesn't after sleep

Posted on October 15, 2014 at 19:38 I'm trying to wakeup the processor after it has been put to sleep by the _wfe instruction via the RTC wakeup event. It is not working for me. There are no examples of WFE wakeup in the library projects tha...

vneff by Associate III
  • 3539 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.