STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

JTAG Boundry scanning

Posted on October 31, 2014 at 13:34Hi:  I have never used JTAG but I understand it has a boundary scan feature that allows testing all the pins for shorts and opens. Also it is possible to JTAG test more than one part by 'daisy chaining' JTAG from ...

sanjib by Associate III
  • 2026 Views
  • 4 replies
  • 0 kudos

USB Host FreeRTOS Assertion fails

Posted on October 31, 2014 at 20:02As soon as the USB disk is connected, I get an assertion fail, with this comment above this assertion:/* The following assertion will fail if a service routine (ISR) for an interrupt that has been assigned a priori...

Johanan1 by Associate II
  • 1013 Views
  • 1 replies
  • 0 kudos

How to connect clock crystal on STM32F427VIT?

Posted on November 02, 2014 at 20:14I am a newbie with ARM and ST parts, but I have used Microchip PIC parts for many years, though. Now I believe is the time to switch to a more powerful and expansive platform, so I am investigating ARM. I download...

bo by Associate
  • 1199 Views
  • 1 replies
  • 0 kudos

stm32f407 - no cortex m sw device

Posted on October 31, 2014 at 14:43Hi, I'm a student starting to develop on my STM32F407 using uVision,I'm struggling on getting my board to link to my pc, I have installed the USB drivers but I still get the error ''no cortex M sw device'' from my ...

Where to report bugs in forum itself?

Posted on November 01, 2014 at 13:57Hi,This forum (seems to be based on MS-sharepoint) has a lot of bugs.For example, I can write new discussion only in Chrome and reply only on IE.When I write a new discussion or reply, I have always to select all ...

Osto by Senior
  • 1279 Views
  • 2 replies
  • 0 kudos

Fluctuations on clkout pin under load

Posted on November 01, 2014 at 10:46I've noticed that the output of the clkout pin is very near the frequency I would expect when a external crystal is used as the pll source, but fluctuates a little as the CPU performs gpio operations. When I confi...

STM32f405RGT6 UART4 and USART3 TX problems

Posted on October 31, 2014 at 12:11I'm at wits end trying to figure out why exactly I can't transmit on UART4 or USART3.The RX works, and i can receive data, however the TX pin is not working at all. Below is my configure code for UART4.void init_us...

tylere by Associate II
  • 2845 Views
  • 5 replies
  • 0 kudos

Phantom Flash Errors

Posted on October 31, 2014 at 13:53 Hi all. I'm working on a project on an STM32L151CBT6 uC, and getting occasional, unexplained error bits WRPERR and SIZERRset in the flash controller. I set up the flash error interrupt to use the highes...

maroot by Associate
  • 1478 Views
  • 2 replies
  • 0 kudos

Init SRam with Zero for SRamParityChecking

Posted on October 31, 2014 at 14:09 I use STM32F030F4 and want to use SRam-parity-checking. The reference manual hints: ''When enabling the RAM parity check, it is advised to initialize by software the whole RAM memory at the beginni...

klaus2 by Associate II
  • 5155 Views
  • 10 replies
  • 0 kudos

F303, nrf24l01 interfacing problems

Posted on October 29, 2014 at 14:19I tried porting someone else's code here:  https://github.com/LonelyWolf/stm32/blob/master/Nrf24l01/nRF24l01.c to F3 (his is for the F1 family).I'm using one of the http://www.addicore.com/2pcs-Addicore-nRF24L01-Wi...

0690X00000605BcQAI.png
arolsen by Associate II
  • 2766 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.