STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Memory-to-Memory DMA transfer to 16-bit SRAM

Posted on November 03, 2014 at 10:17I have an STM32F429 connected via FMC to a 16-bit wide SRAM. I can read and write to the SRAM correctly using simple memory writes.DMA works correctly too when I configure it with two streams; one to send internal...

dohzer by Associate II
  • 5358 Views
  • 5 replies
  • 0 kudos

Help targeting an STM32F4DISCOVERY

Posted on November 20, 2014 at 19:11Hi everyone, I am trying to download some code onto a development board and I know for sure that the code itself works correctly. But I'm getting an error saying that I haven't targeting the board correctly so I w...

Bluetooth HC-05 and STM32F4 Discovery

Posted on November 20, 2014 at 00:50 Hello i want to test my BT on Discovery board. I connected all pins correctly and build easy code for recive data and turn on the light.In my code i use this function to recive data on STM. if (USA...

samotan by Associate II
  • 1692 Views
  • 4 replies
  • 0 kudos

STM32F2xx RTC: LSE Jitter problem

Posted on November 18, 2014 at 15:38Hello to all, For calibration I use Timer 5 Capture-Channel4 to measure the LSE Clock on a STM32F207 CPU. However the result was variing +- 20 Hz. To deviate external crystal issues I routed LSI to the Timer 5 cap...

andywild2 by Associate III
  • 2353 Views
  • 8 replies
  • 0 kudos

Do you use STM32cubeMX

Posted on November 19, 2014 at 19:39Hello,ST announced that everybody should use the cubeMX software (or at least libraries) because the old libraries will not be supported anymore. I was a noob on STM32 so I decided to start with cubeMX.It it clear...

tarzan2 by Senior
  • 2258 Views
  • 6 replies
  • 0 kudos

sdio fatfs speed problem

Posted on January 22, 2014 at 20:31i use fatfs and i read at about 200to300KB/SECOND  it's very low speed . i test sd card speed from computer and it's speed reading 12.5MB/SECOND how to speed up sd card reading i want about 5MB/sec are this hard ...

elec_st by Associate III
  • 4903 Views
  • 25 replies
  • 0 kudos

STM32L0xx Altium Files

Posted on November 20, 2014 at 16:44Hi, Are STM32L0xx files (sch, lib, ref design) for Altium Designer available somewhere for download? In order to go quickly and avoid error..... Thanks

STM32F407: Strange Idle/RXNE on UART4-5 (not on USART1-3/6)

Posted on November 20, 2014 at 12:30Hi, I found a very strange behaviour for the UARTs: The IDLE Flag of UART4-5 will ''extinguish'' after typically 100-500msec (Baudrate 100kB and 9600). I tried with 2 Discovery boards and with all UARTs. The ''sy...

flyer31 by Senior
  • 1104 Views
  • 3 replies
  • 0 kudos

volatile variables and ''functions''

Posted on November 20, 2014 at 11:48 Hello, i am running compile (IAR AMR) in highest optimization settting, but sometimes it does ignores my code, or even functions that does have purpose; as example, DataRx[] is loaded by DMA with ...

Nucleo STM32F334R8 DAC

Posted on October 23, 2014 at 14:05Hello community,Actually I evaluating DAC on NucF334R8. DAC1_Channel1 seems to work but I am not able getting DAC2_Cannel1 (Pin PA6) to work. I created the C Framework with STMCubeMX 4.4.0 - both channels with equa...

0690X00000605OxQAI.png
heap by Associate II
  • 4593 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.