STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Code size generation

Posted on November 21, 2014 at 18:47Hi all,I´m developing an application in Keil uVision with STM32L052C that is a uC that has 32KB of flash memory.I add my ST libraries and per example STM32L0xx_hal_uart.c. This library uses some features with DMA ...

gerardo by Associate II
  • 1227 Views
  • 2 replies
  • 0 kudos

Pb generating 2 PMW

Posted on November 21, 2014 at 12:04The original post was too long to process during our migration. Please click on the attachment to read the original post.

franck2 by Associate II
  • 8819 Views
  • 22 replies
  • 0 kudos

Locate Heap in SDRAM

Posted on November 20, 2014 at 15:39Hello, I have STM32f429 discovery board and I want to locate heap in SDRAM. SDRAM adress is 0xD0000000, size 0x800000. I use the Keil uvision 4. How to configure Keil and my code? #understand-your-tools #stm32...

z1060 by Associate II
  • 3228 Views
  • 5 replies
  • 0 kudos

stm32f3 discovery Gyroscope issue (L3GD20)

Posted on November 20, 2014 at 21:22 Hi guys, I am working on the L3GD20 embeeded in the stm32f3 discovery board. I came with this code which gives me 0 on the 3 axes even when i move the board. any suggestions please? #include '...

d4ng3r09 by Associate II
  • 1597 Views
  • 2 replies
  • 0 kudos

STM32 Nucleo Firmware Source code (STSW-LINK007)

Posted on November 21, 2014 at 00:44Hi, we are developing a couple of STM32 boards. Want to target the mbed platform. For programming, we would like an optional small daughter board that can plug into our board, that provides the programming/debuggi...

Problem with multiblock SDIO read/write on F1 & F4

Posted on January 03, 2013 at 22:11Hi everyone,Whenever I use either of the multiblock read/write functions the peripheral gets stuck in the SD_CARD_SENDING or SD_CARD_RECEIVING state, respectively. Further attempts to access the peripheral in this ...

stm32f0 discovery CAN bit timing

Posted on November 19, 2014 at 17:29Hello,I'm having problems with bit timing configuration. I have 36MHz peripheral clock and need 500kBit/s on CAN. I'm having trouble, because I've calculated right value but I see on the oscilloscope that it isn't...

urban by Associate
  • 1536 Views
  • 3 replies
  • 0 kudos

WakeUp from STOP using an EXTI GPIO LINE

Posted on November 19, 2014 at 17:07I am having trouble to wake up the STM32F407 from the STOP condition using a GPIO EXTI line (PB 0).   The same GPIO line is used when the STM32 is ON to switch it OFF (THIS WORKS PERFECTLY) and whenever it is OFF ...

STM32f405 spi trouble with LSM9DS0

Posted on November 08, 2014 at 03:50the i-nemo forum is a little slow hopefully maybe i can get a faster answer here...I'm trying to interface with the LSM9DS0 and I can't get any coherent information from it. when I try to read the who am I registe...

tylere by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.