2015-01-06 2:01 AM
I am a newbie to STM32. I would like to migrate existing solution to STM32 which uses a button library that can detect double-press, triple-press, long-press, very-long-press etc.
Is there a button library available for the STM32 platform that I can use?Thank you very much.2015-01-06 4:09 AM
I have never seen a library like that, but it could be written quite easily.
My usual pushbutton filtering code is//Key is pressed when ''Keyfilter'' goes up to 10, and released if counts down to 0. Counting +/-1 happens at every 1 msec.
#define KEY_FILTER_MAX 10 if (GPIO_ReadInputDataBit (<port, bit>)==0) { Keyfilter++; } else { Keyfilter--; } if (Keyfilter < 0) { Keyfilter= 0; //stuck at lower limit } if (Keyfilter > KEY_FILTER_MAX) { Keyfilter= KEY_FILTER_MAX; //limit at max value } if ((Keyfilter == 0) && (KeyServiced != 0)) { //if it have been reported, but not held down any more, we do service for release KeyServiced= 0; KeyReleaseService(); } if ((Keyfilter == KEY_FILTER_MAX) && (KeyServiced == 0)) { //it is pushed but not serviced yet KeyPressTime= T_msec; KeyServiced= 1; KeyPressService(); } } If you push key-state-change-times into an array of 6 element (oldest item is to be shifted out: last 6 up/down times are stored), you can detect double/triple strokes: I evaluate buffer if last pushed item is a release event. At evaluate function - I check the time difference of the actual release and the previous down event. If it is shorter than 10msec, it's a glitch only. If it is 10msec..0.5sec, then normal push, if >0.5sec then a long push. - I check the time and duration of [last-2] and [last-3] element pair...if they are older than 1sec, then they are part of a different sequence...if newer than 1sec, it's double (or triple) press ..and so on...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.