STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB data buffer overlaps with stack leading to fault

Posted on January 25, 2015 at 10:27Hi,I am running a USB MSC project on my STM32L1 board generated using the CubeMX software.I am noticing that during enumeration, the device receives a Read10 request for 16 blocks of data (each 512 bytes in size). ...

bnp979 by Associate III
  • 2043 Views
  • 3 replies
  • 0 kudos

STM32F4xx HAL UART BAUD Timing Issues

Posted on January 24, 2015 at 19:54 Hi there... Using the non-hal on an STM32F2xx, I can read/write at 3,333,333 BAUD without a problem. When I port the code to STM32F4xx, I am unable to read/write to the USART1 at the same BAUD rate - instead, ...

dj by Associate II
  • 1157 Views
  • 1 replies
  • 0 kudos

Classroom development dilema

Posted on January 14, 2015 at 17:51I am teaching a course on embedded programming and am having some logistics issues I am hoping someone might be able to help with here.I have taught a class using the STM32F3 before but I had a linux environment av...

aes by Associate II
  • 3862 Views
  • 9 replies
  • 0 kudos

STM32F072 Discovery as programmer

Posted on January 23, 2015 at 10:27I have just gotten the PCB for my first STM32-based design, using a F072CBT6 chip. The board is only populated with the power regulator and the CPU with its surrounding passive components. I have the F072 Discovery...

jesper by Associate II
  • 1679 Views
  • 2 replies
  • 0 kudos

Efficient I2S operation with MONO Audio

Posted on January 25, 2015 at 09:02I'm experimenting with an audio ADC connected to the I2S peripheral on my STM32F401 Discovery Board. Right now I have the microcontrollers I2S interface configured as slave half-duplex mode (input only). In other w...

STM32F303 PWM

Posted on January 24, 2015 at 17:52 Hello, i have a problem with PWM. I am trying to turn on the led (PE9) on TIM1_CH1. I want to make it brighter and brighter till counter equals 256 (2^8=256) #include < stm32f30x.h > #include <...

deredas1 by Associate
  • 1240 Views
  • 2 replies
  • 0 kudos

USART communication between stm32f407 and two stm32f030

Posted on January 21, 2015 at 09:55HI ALL I have written a code for USART communication  full duplex between stm32f407 and stm32f030 and it is working fine as soon as power on reset. The half duplex communication also working fine between two stm32f...

sanjib by Associate III
  • 4447 Views
  • 11 replies
  • 0 kudos

STM32F4 Discovery no I/O toggle

Posted on March 29, 2014 at 19:51I am trying to toggle an I/O line to measure timing for benchmarking dsp algorithms on an STM32F407VGT. I generated the HAL using STM32CubeMX and set PD12 and PC8 to outputs and configured them as output push-pull wi...

sc2 by Associate II
  • 3804 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.