STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fix for STM32F0xx StdPeriph Lib

Posted on July 21, 2014 at 15:54 Hello, I just ran into a trap with STM32F0xx_StdPeriph_Lib_V1.3.1 and have a suggestion for a fix. In function ADC_ChannelConfig() of file stm32f0xx_adc.c, the line 724 ADCx->CHSELR |= ...

oliver by Associate
  • 1139 Views
  • 1 replies
  • 0 kudos

Unable to receive CAN data

Posted on September 08, 2014 at 23:47I am working on the STM32F302 Micro and I currently unable to receive data on the CAN bus, I have a break point set on the interrupt routine.  I am able to transmit data.  I am seeing the micro sends an acknowled...

ebommer by Associate II
  • 4605 Views
  • 10 replies
  • 0 kudos

Heavy mechanical shocks STM32F405RG

Posted on January 21, 2015 at 19:27Hello there!I need to develop the device which has to sustain heavy mechanical shocks (a peak of 10 000g). I am going to use http://www.ti.com/product/MSP430F5438A-EPSTM32F405RG. What level of mechanical shock can ...

wersalec by Associate
  • 1938 Views
  • 3 replies
  • 0 kudos

timer can't be disabled

Posted on January 26, 2015 at 14:26Dear all,I face a strange behaviour of a timer. I appreciate any comments and suggestions.The timer is configured in one pulse mode and with slave mode 'trigger' from channel 1. With a rising edge the timer is trig...

4x4 KEYPAD

Posted on January 25, 2015 at 15:514x4 KEYPAD

kemal by Associate II
  • 795 Views
  • 1 replies
  • 0 kudos

STM32F205RCTb USB OTG FS :Is Pull up required on DP

Posted on January 25, 2015 at 18:13We are using USB FS ( PA11 / PA12 ) in device mode. We have grounded ID pin i.e. PA 10 .We have not used any Pull up or pull down on DP and DM pin  as described in eval board schematics STM32 20-21-45-46 G-EVAL USB...

jagbir by Associate
  • 1556 Views
  • 2 replies
  • 0 kudos

DMA2 Not getting interrupt

Posted on February 24, 2014 at 16:42The original post was too long to process during our migration. Please click on the attachment to read the original post.

ch2 by Associate III
  • 8094 Views
  • 21 replies
  • 0 kudos

STM32F429 SDRAM unreliable

Posted on October 20, 2014 at 02:18I've copied the SDRAM hardware and software from the STM32F429 Discovery board. We've made a few boards so far. On some the SDRAM doesn't seem to work at all while on others it seems to work for a bit then get corr...

peterm by Associate II
  • 3146 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.